STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 TFT Swipe

Posted on May 29, 2016 at 12:55Hi,I'm using STM32F429 with tft of 640X480 with touch.I want to simulate the effect of screen swipe – as in Smartphone: When the user swipe it's finger the screen is moving to that direction and another screen is enter...

doron by Associate
  • 698 Views
  • 0 replies
  • 0 kudos

STM32F4 TFT Swipe

Posted on May 29, 2016 at 12:51Hi,I'm using STM32F429 with tft of 640X480 with touch.I want to simulate the effect of screen swipe – as in Smartphone: When the user swipe it's finger the screen is moving to that direction and another screen is enter...

doron by Associate
  • 631 Views
  • 0 replies
  • 0 kudos

STM32Fy46G-DISCO SAI with DMA

Posted on May 29, 2016 at 10:06hello. I make audio player on STM32F7-DISOC. I want to use SAI with DMA transfer. Using STM32CubeMX and stm32746g_discovery_audio.c of STM&sharp2CubeF7 and reffeing to Audio_playback_and_record project. SAI and DMA se...

hayandu by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

Need help with CAN controller

Posted on May 27, 2016 at 20:11 Hi, i m using STM32F103 nucleo board. I m configuring CAN controller to receive particular message ID for Standard Identifier (CAN ID : 0x0212) Here is my configuration for acceptance filter. CAN_...

SS.Sagar by Associate III
  • 1091 Views
  • 2 replies
  • 0 kudos

STM32F407: SPI as slave using DMA

Posted on May 27, 2016 at 17:31 Hi there, I'm desperatly trying to get the STM32F407 work as a SPI slave with DMA TX/RX functionality. I literally read any thread about this topic Google found (~5 pages of results) but it's just not work...

STM32F4: Using several ADCs independent

Posted on May 28, 2016 at 12:59Hello, I wonder if it is or it is not possible to use more than one ADC independet of each other. My problem is as follows: I want to use ADC1 and ADC2 in dual mode and ADC3 in independent scan conversion mode. I can s...

STM32F767 examples / support

Posted on May 03, 2016 at 14:08Hi,any idea when support for these is out? I've got a 767ZI... I whacked on a nucleo board and would like to check out some DP FPU stats,regards 

tau by Associate II
  • 3687 Views
  • 14 replies
  • 0 kudos

Interrupt on PE2 not working

Posted on May 27, 2016 at 20:49Hi, I'm working on a STM321F407IG MCU and trying to get interrupt working on pin PE2. I'm using HAL Library and got INterrupts Working on some of the other pins but not on PE2. In GPIO Configuration I set Mode of the ...

RTC_CR Daylight Saving

Posted on May 26, 2016 at 18:05 Hello, Looking at the RM0090, I can read on the RTC_CR register description : Bit 17 SUB1H: Subtract 1 hour (winter time change) When this bit is set outside initialization mode, 1 hour is subtracte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.