2020-09-09 8:10 PM
I believe the QSPI Flash memory is in the memory mapped mode on the DISCO board. I programmed a 2KB bin file into the flash memory using the ST Link utility. I want to read this to internal ram. I set this project up with CubeMX. Can I change the flash memory to direct mode on this DISCO board. Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.