2012-11-23 5:34 AM
hello,
my stm32f4discovery board started not working without connecting external 0-5V power supply to GND and 5V pins.when i plug usb only, nothing happens, none of the leds light. if i connect external power additionally, it connects to pc and i can even programme mcu.all of this happened after shorting two pins unintentionally while making connections.how can i solve this problem?thanks. #stm32f4discovery #power2012-11-23 6:15 AM
how can i solve this problem?
Figure out which parts in the power supply path you have destroyed and replace them. Get the schematic and a multi-meter/scope.2012-11-23 6:19 AM
which parts are related with power on Discovery board? does it include something like a fuse?
2012-11-23 7:29 AM
which parts are related with power on Discovery board? does it include something like a fuse?
Do you see a fuse in the schematic? I'd look at D1 as the first candidate for silicon evaporative protection. Here's the schematic/manual if you're having a hard time finding it.http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00039084.pdf
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.