2021-10-28 11:10 AM
Hi all
My USB Camera support YUY2 & MJPEG format, PC read back the correct configuration, but STM32 not correct, the configuration only contain MJPEG format! And the other infomation seems correct. Why camera can distinguish the PC and STM32 host ?
I have attached the full configuration from PC & STM32, please have a look.
And even though I use the MJPEG to capture frame, evering is OK, but when I start a transfer, I can only receive SOF interrupt and 'USB_OTG_GINTSTS_PXFR_INCOMPISOOUT' interrupt, which mean 'Incomplete periodic transfer '. I don't why this happens, what should I do next.
Many thanks for your help!
2021-10-28 11:17 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.