2013-12-04 11:29 AM
Hello,
Today I bought one of these new stm32f429 discovery boards :http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090
For the moment I only launched the demo software, but it seems that the tuchscreen is abnormally inaccurate (less precise than the one of my colleage). For example in the calendar, when my pen is on the 22 of the month, the red square moves between the 18 ant the 21.Has someone experienced the same problem ? Is there a way to callibrate the touchscreen ?Some pins were creased when I got the board, could a shock during transport have killed the touchscrean ? (In this case I will try to exchange the board) #stm32f4 #discovery #stm32f4292013-12-05 6:13 PM
The adjustment can be made in software by scaling based on knowing 5 points. The four corners and centre.
One might want to look in STM32F429I-Discovery_FW_V1.0.1\Utilities\STM32F429I-Discovery\stm32f429i_discovery_ioe.c At routines IOE_TP_Read_X(), IOE_TP_Read_Y(), and IOE_TP_Read_Z() The screen tends to separate from the board as the cable is trapped underneath, and springs upward, the metal casing has two double-sided tape strips (1/4'') down the long sides adhering it to the board. The plastic frame can also separate from the metal shell, which contacts about 2/3 of the length, with punch outs to trap nubs on the plastic. The screen also ships with a plastic film over it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.