2014-01-16 12:40 AM
Hi all,
I am looking for a little help about loading and displaying a simple picture on the LCD of this ev-board, without the need of an-OS: just to make a picture after power-on. I have found a few examples of drawing basic figures, how to convert pictures to hex data and include them in a C file, but the next steps are quite blurry: DMA2D is quite too complex for me at the moment... Can STemWin could be helpful ? Do you have some example code ? Thanks2014-01-16 8:48 AM
There's this
http://www.st.com/web/en/catalog/tools/PF259429#
And the stuff located in STM32F429I-Discovery_FW_V1.0.1\Projects\Demonstration\Core I've got the materials from the seminar too, but the whole thing runs about 1GB and uses IAR, so I'm not going to post a link to it here. I'll have to see if the graphic stuff breaks out easily, or is materially different from the demo stuff cited.2014-01-17 6:56 AM
I downloaded the STM32F429I-Discovery_FW_V1.0.1 archive and had a look on some folders, thanks a lot !
I am going to dig deeper in, but it seems they're using STemWin !? RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.