2016-11-15 9:42 PM
Hello,
I am trying to configure pins D0-D15 on the STM32F429VIT6 to output sram data. The code seems to be functioning properly and I have scoped out each of the pins however Pin44(PE13)-D10 seems to never go high. Configuring the pin to gpio allows it to toggle on and off. Is it possible to damage an alternate function on a pin? Below is the GPIO init code.void SRAM_GPIOConfig(){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; /* Common GPIO configuration */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; /* GPIOD configuration */ GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FMC); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init(GPIOD, &GPIO_InitStructure); /* GPIOE configuration */ GPIO_PinAFConfig(GPIOE, GPIO_PinSource0 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource1 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource3 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource4 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource7 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource8 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource9 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource10 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource11 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource12 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource13 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource14 , GPIO_AF_FMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource15 , GPIO_AF_FMC); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init(GPIOE, &GPIO_InitStructure);}2016-11-16 2:32 PM
Ok, with the load disconnected, checked the GPIOD & E registers and they are setup correctly. I also ported the same code to the F4Disco board and it worked on all pins. I am a bit clueless as to whats going on now if a hardware issue is very unlikely. I am using the Periph v1.2 library on both targets.
2016-11-16 3:33 PM
The 'F429 DISCO, or the 'F407 DISCO?
Is there anything else connected to the FMC,e.g. a SDRAM? Did you go through the FMC errata? There are quite a few of them, although most of them for specific scenarios. The LCD peripheral is on or off? I'd assume off, given the small package, but I though to ask just to be sure (it should not collide but one never knows). (Btw, why not the '427?) Any other peripheral enabled, even a seemingly unrelated one (such as USB, or ADC/DAC)? Did you try the GPIO-wiggling while everything else is initialized as in the case in question (except this particular pin), or was it a minimal test program? JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.