2016-11-15 9:27 PM
Hello!Sir:
I have a project which is the MCU(STM32F427) to drive the camera module(OV5642) and referenced the arduino web site (https://github.com/ArduCAM/Arduino/tree/master/ArduCAM) to setup the register value for the VGA_preview_setting, Video_setting...etc.My firmware has a error which is the ''DCMI_DR_ADDRESS'' undefined after compiling.#define QVGA_resolution 320*240uint32_t frame_buffer[QVGA_resolution];void OV5642_Config_DCMI_DMA(ImageFormat_TypeDef ImageFormat){ DCMI_InitTypeDef DCMI_InitStructure; DMA_InitTypeDef DMA_InitStructure; /*** Configures the DCMI to interface with the OV5642 camera module ***/ /* Enable DCMI clock */ RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_DCMI, ENABLE); /* DCMI configuration */ DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMode_Continuous; DCMI_InitStructure.DCMI_SynchroMode = DCMI_SynchroMode_Hardware; DCMI_InitStructure.DCMI_PCKPolarity = DCMI_PCKPolarity_Rising; DCMI_InitStructure.DCMI_VSPolarity = DCMI_VSPolarity_Low; DCMI_InitStructure.DCMI_HSPolarity = DCMI_HSPolarity_Low; DCMI_InitStructure.DCMI_CaptureRate = DCMI_CaptureRate_All_Frame; DCMI_InitStructure.DCMI_ExtendedDataMode = DCMI_ExtendedDataMode_10b;//data =8b/10b? /* Configures the DMA2 to transfer Data from DCMI */ /* Enable DMA2 clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE); /* DMA2 Stream1 Configuration */ DMA_DeInit(DMA2_Stream1); DMA_InitStructure.DMA_Channel = DMA_Channel_1; DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) frame_buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 1; //DMA_InitStructure.DMA_BufferSize = 320; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;}1.How to solve the error message?2.Does the parallel data is 8 bits or 10bits for OV5642?3.Who can support the OV5642 sample code for me referenced?4.DMA_BufferSize=pixel /4 ?5.DMA_Memory0BaseAddr= frame_buffer array address?2016-11-16 7:39 AM
Do you define DCMI_DR_ADDRESS anywhere in your code, or where you took it from?
Would &DCMI->DR suffice to get the address?The size of the DMA buffer is in Transfer units, and you'd likely want the memory address to increment to fill the buffer. You'd probably want to decide on Word or Half-Word.Not sure there are a wealth of people here supporting ArduCAM or DCMI, you might want to thoroughly review the manual, and the examples within the SPL.2016-11-16 6:21 PM
Hi!Clive1:
I have fixed this error message yesterday as the blow shown that the item 1 and 21.#define DCMI_DR_ADDRESS 0x50050028 DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_Address; 2.DMA_InitStructure.DMA_PeripheralBaseAddr =(uint32_t)(DCMI_BASE + 0x28); But I have the below questions are that I don't understand.2.Does the parallel data is 8 bits or 10bits for OV5642?3.Who can support the OV5642 sample code for me referenced?4.DMA_BufferSize=pixel /4 ?5.DMA_Memory0BaseAddr= frame_buffer array address?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.