STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which API use for RTOS?

Posted on November 17, 2016 at 12:57Hello, The STM32cubeMX code generator labels as FreeRTOS the RTOS functionalities, but the code generated looks compliant to the CMSIS-RTOS API. The directory Middlewares\Third_Party\FreeRTOS\Source contains the s...

HELP_STM32F4DIS and HC SR04

Posted on November 17, 2016 at 14:26 I comunicate stm32f4dis with hc sr04 but always distance_mm=0, PB1-Trig PB0-Echo #include ''stm32f4xx.h'' GPIO_InitTypeDef GPIO_InitStructure; void GPIO_Configuration( void ); void ...

kakaducsy by Associate II
  • 1261 Views
  • 0 replies
  • 0 kudos

STM32F103 xl option bytes

Posted on November 17, 2016 at 13:39I'm unable to program the option bytes from user software. In an STM32F103RGT7.Erase works, program does not.Code:// Lock and unlockFLASH->CR = FLASH_CR_LOCK;if( FLASH->CR & FLASH_CR_LOCK ){  // Unlock fpec       ...

Jeroen3 by Senior
  • 964 Views
  • 0 replies
  • 0 kudos

STemWin

Posted on September 07, 2016 at 23:27Hi, I wonder if there is any chance for stemwin 5.30 or newer in near future ?Thanks

How to configure GPIO input?

Posted on November 14, 2016 at 21:35Good day,What I want is: If I put GND to GPIOD_4 I want to LED ON.If high impedance then LED OFF.I attached my schematic with CHRG pin connected to GPIOD_4.Is it possible to pull up internally gpio?I wrote some co...

hitsumen by Associate II
  • 2136 Views
  • 2 replies
  • 0 kudos

Position Independent Code Support(PIC) on STM32F479NI

Posted on November 16, 2016 at 13:18We are trying to implement Position Independent Code (PIC) on STM32F479NI. We have used -fpic and -msingle-pic-base options while compiling the code. Initially we wanted prove that this PIC concept will work on a ...

jitheesh by Associate
  • 1200 Views
  • 2 replies
  • 0 kudos

DMA Issue for STM32F427 and OV5642

Posted on November 16, 2016 at 06:27Hello!Sir:I have a project which is the MCU(STM32F427) to drive the camera module(OV5642) and referenced the arduino web site (https://github.com/ArduCAM/Arduino/tree/master/ArduCAM) to setup the register value fo...

pohua by Associate II
  • 1556 Views
  • 2 replies
  • 0 kudos

STM32F429 Dead alternate function on pin?

Posted on November 16, 2016 at 06:42Hello,I am trying to configure pins D0-D15 on the STM32F429VIT6 to output sram data. The code seems to be functioning properly and I have scoped out each of the pins however Pin44(PE13)-D10 seems to never go high....

USB communication on Nucleo-64 STM32F401RE

Posted on November 16, 2016 at 10:25Hi,Currently I implemented SPI communication to external device using Nucleo-64 stm32f401RE.SPI implementation is based on Bit banding and not the HW SPI.Clk rate is ~3.2MHzSince the Nucleo-64 is used to communica...

nirb by Associate II
  • 2714 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.