2018-01-17 4:00 AM
Hello,
i am using STM32F429IIT controller.I am trying communicate between CAN1 and CAN2 but yet not success.can you please provide any reference code for the CAN communication.
Thanks
#stm32f429-can-communication2018-01-17 5:04 AM
yet not success
What is the exact problem?
please provide any reference code
Check CubeMX examples repository.
2018-01-17 5:22 AM
It is as likely that you haven't wired it up appropriately.
Provide context about what you are currently trying, both code and physically connectivity. This will save a lot of time in understanding and explaining the problem.
I have previously posted code for the RedDragon 407 board demonstrating CAN1 to CAN2 comms on the platform.
2018-01-17 12:36 PM
the CAN Rx input pins must be pulled high.
Are you using a driver chip ?
2018-01-17 8:46 PM
I followed procedure on
https://www.youtube.com/watch?v=GYhsHJi6pKE
by this code my program stop in while loop of CAN2_RX
uint8_t CAN2_RX(void)
{ while(!hcan2.Instance->RF0R & CAN_RF0R_FMP0);//CAN_RF0R_FMP0 FOR 3 uint8_t RxD=(hcan2.Instance->sFIFOMailBox[0].RDLR)&0xFF; hcan2.Instance->RF0R|=CAN_RF0R_RFOM0;//CAN_RF0R_RFOM0 FOR 1<<5 return RxD;}i received only first byte in sFIFOMailBox[0].RDLR i.e RxD.
My physical hardware connection is also ok . i have checked on scope i am receiving data(waveform) on both side
Here is the my code
Header 1
CAN_HandleTypeDef hcan1;
CAN_HandleTypeDef hcan2;uint8_t k, RxData;void CAN1_TX(uint8_t data){ hcan1.Instance->sTxMailBox[0].TDLR=data; hcan1.Instance->sTxMailBox[0].TIR|=1;//CAN_1TI0R_TXRQ FOR 1}uint8_t CAN2_RX(void){ while(!hcan2.Instance->RF0R & 3);//CAN_RF0R_FMP0 FOR 3 BMS_MASTER_GREEN_LD_ON; uint8_t RxD=(hcan2.Instance->sFIFOMailBox[0].RDLR)&0xFF; hcan2.Instance->RF0R|=1<<5;//CAN_RF0R_RFOM0 FOR 1<<5 return RxD;}int main (void){ HAL_Init(); SystemClock_Config(); MX_CAN1_Init(); MX_CAN2_Init(); hcan1.Instance->sTxMailBox[0].TIR=(uint32_t)0; hcan1.Instance->sTxMailBox[0].TIR=(uint32_t)(0x245<<21)|CAN_ID_STD; hcan1.Instance->sTxMailBox[0].TIR|=CAN_RTR_DATA; hcan1.Instance->sTxMailBox[0].TDHR&=~CAN_TDT0R_DLC; hcan1.Instance->sTxMailBox[0].TDTR|=(1&CAN_TDT0R_DLC); hcan1.Instance->FMR|=1<<0; hcan1.Instance->FMR|=14<<8; hcan1.Instance->FS1R|=1<<14; hcan1.Instance->sFilterRegister[14].FR1=0x245<<21; hcan1.Instance->FM1R|=(uint32_t)(1<<14); hcan1.Instance->FA1R|=1<<14; hcan1.Instance->FMR&=~((uint32_t)CAN_FMR_FINIT); while(1) { k++; if(k>25) k=0; CAN1_TX(k); RxData=CAN2_RX(); HAL_Delay(1000); }}static void MX_CAN1_Init(void){ hcan1.Instance = CAN1; hcan1.Init.Prescaler = 16; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_3TQ; hcan1.Init.BS2 = CAN_BS2_5TQ; hcan1.Init.TTCM = DISABLE; hcan1.Init.ABOM = DISABLE; hcan1.Init.AWUM = DISABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}/* CAN2 init function */static void MX_CAN2_Init(void){ hcan2.Instance = CAN2; hcan2.Init.Prescaler = 16; hcan2.Init.Mode = CAN_MODE_NORMAL; hcan2.Init.SJW = CAN_SJW_1TQ; hcan2.Init.BS1 = CAN_BS1_3TQ; hcan2.Init.BS2 = CAN_BS2_5TQ; hcan2.Init.TTCM = DISABLE; hcan2.Init.ABOM = DISABLE; hcan2.Init.AWUM = DISABLE; hcan2.Init.NART = DISABLE; hcan2.Init.RFLM = DISABLE; hcan2.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}2018-01-17 8:50 PM
Here is the my can init function
static void MX_CAN1_Init(void)
{hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 16; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_3TQ; hcan1.Init.BS2 = CAN_BS2_5TQ; hcan1.Init.TTCM = DISABLE; hcan1.Init.ABOM = DISABLE; hcan1.Init.AWUM = DISABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
/* CAN2 init function */
static void MX_CAN2_Init(void){hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 16; hcan2.Init.Mode = CAN_MODE_NORMAL; hcan2.Init.SJW = CAN_SJW_1TQ; hcan2.Init.BS1 = CAN_BS1_3TQ; hcan2.Init.BS2 = CAN_BS2_5TQ; hcan2.Init.TTCM = DISABLE; hcan2.Init.ABOM = DISABLE; hcan2.Init.AWUM = DISABLE; hcan2.Init.NART = DISABLE; hcan2.Init.RFLM = DISABLE; hcan2.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
/**********************************/
void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hcan->Instance==CAN1) { /* USER CODE BEGIN CAN1_MspInit 0 *//* USER CODE END CAN1_MspInit 0 */
/* Peripheral clock enable */ HAL_RCC_CAN1_CLK_ENABLED++; if(HAL_RCC_CAN1_CLK_ENABLED==1){ __HAL_RCC_CAN1_CLK_ENABLE(); } /**CAN1 GPIO Configuration PB8 ------> CAN1_RX PB9 ------> CAN1_TX */ GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP;//GPIO_NOPULL;// GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF9_CAN1; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* USER CODE BEGIN CAN1_MspInit 1 */
/* USER CODE END CAN1_MspInit 1 */
} else if(hcan->Instance==CAN2) { /* USER CODE BEGIN CAN2_MspInit 0 *//* USER CODE END CAN2_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_CAN2_CLK_ENABLE(); HAL_RCC_CAN1_CLK_ENABLED++; if(HAL_RCC_CAN1_CLK_ENABLED==1){ __HAL_RCC_CAN1_CLK_ENABLE(); } /**CAN2 GPIO Configuration PB13 ------> CAN2_TX PB5 ------> CAN2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF9_CAN2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* USER CODE BEGIN CAN2_MspInit 1 */
/* USER CODE END CAN2_MspInit 1 */
}}
2018-01-18 9:29 AM
can any one tell what should be wrong with above code..
2018-01-18 11:42 AM
I think I'd avoid the register level coding until you have the HAL equivalent for RX/TX working.
Look at the available HAL examples, like
STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Examples\CAN\CAN_Networking\Src\main.c
2018-01-18 2:47 PM
hcan.Init.ABOM = ENABLE;
2018-01-19 8:37 PM
thank you so much now it's working fine.
can i transmit(initiate) the CAN communication from CAN slave mode port to CAN master port.and how?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.