2018-01-09 5:50 AM
Hello, this concerns CubeH7 1.1.0.
Simple app with 2 FreeRTOS tasks:
task #1 sends data continously via Ethernet
task #2 calls i.e.
int waiting_time=0x1000;
HAL_SPI_Receive(&hspi2,buf,10,waiting_time);
to receive 10 bytes or whatever.
Thers is no SPI client connected.
The first task is affected by the waiting time and waits as well, no RTOS behaviour anymore !
The delay depends on the waiting time.
This does not happen when using SPI3 (both are identical)
HAL_SPI_Receive(&hspi3,buf,10,waiting_time);
- Joerg -
Solved! Go to Solution.
2018-01-20 6:58 AM
CubeMX 4.23.0 sets 200 MHz as a default for SPI1,2,3 and this is a trap for beginners.
There is no limit test like for STM32F7 series.
The APB1 bus has a maximum frequency of 100 MHz.
Solution: Set DIVQ1 = 8 (old =4)
2018-01-20 6:58 AM
CubeMX 4.23.0 sets 200 MHz as a default for SPI1,2,3 and this is a trap for beginners.
There is no limit test like for STM32F7 series.
The APB1 bus has a maximum frequency of 100 MHz.
Solution: Set DIVQ1 = 8 (old =4)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.