2024-10-20 1:42 AM - last edited on 2024-10-21 8:33 AM by mƎALLEm
I am currently using STM32CubeIDE and want to input an external sine wave. The signal has a voltage of 2.6V and a frequency of 10kHz, and I am using DMA + TIM + ADC. The following is the screenshot of my settings.
Currently, I can only capture the peak value of 2.6V, and this is only achievable when the ADC Sampling Time is set to 480 Cycles. With a lower number of cycles, I can only get lower values. Please help me resolve this issue, thank you!
DMA:
ADC:
TIM:
Clock Configuration:
Below is my code:
///////////////ADC////////////////
int test = 0;
uint32_t lastTick = 0;
uint16_t ADC_Value[4095] = {0};
float ADC_MaxValue = 0;
float ADC_MinValue = 0;
int count = 0;
double ADC_Value_Sum = 0;
int ADC_Value_AVG = 0;
float clock_AVG = 0;
uint16_t max_value = 0;
uint16_t min_value = 0;
char buffer[20];
HAL_TIM_Base_Start(&htim2);
/* USER CODE BEGIN WHILE */
while (1)
{
if (uart_received)
{
uart_received = 0;
if (uart_command == 'A')
{
check = 1;
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)ADC_Value, 4095);
}
else if (uart_command == 'Z')
{
check = 0;
m = 10000;
ADC_Value_Sum = 0;
memset(ADC_Value, 0, sizeof(ADC_Value));
HAL_ADC_Stop_DMA(&hadc1);
count = 0;
high_time_Sum = 0;
count_phase = 0;
zero_remove = 0;
max_value = 0;
min_value = 0;
}
else if (uart_command == 'S')
{
check = 2;
}
}
if (adc_conversion_complete)
{
adc_conversion_complete = 0;
sprintf(buffer, "Max: %.3f V, Min: %.3f V\r\n", ADC_MaxValue, ADC_MinValue);
HAL_UART_Transmit(&huart1, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY);
}
if (check == 1)
{
if (HAL_GetTick() - lastTick >= 50000)
{
m += 10000;
ADC_Value_Sum = 0;
memset(ADC_Value, 0, sizeof(ADC_Value));
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)ADC_Value, 4095);
lastTick = HAL_GetTick();
}
ad9850_wr(0x00, m);
}
else if (check == 0)
{
ad9850_wr(0x00, 0);
}
else if (check == 2)
{
ad9850_wr(0x00, m);
}
}
/* USER CODE END WHILE */
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
if(TIM2 == htim->Instance){
if(HAL_TIM_ACTIVE_CHANNEL_1 == htim->Channel){
switch(capture_cnt){
case 1:
capture_buf[0] = __HAL_TIM_GET_COMPARE(htim,TIM_CHANNEL_1);
__HAL_TIM_SET_CAPTUREPOLARITY(htim,TIM_CHANNEL_1,TIM_INPUTCHANNELPOLARITY_FALLING);
capture_cnt++;
break;
case 2:
capture_buf[1] = __HAL_TIM_GET_COMPARE(htim,TIM_CHANNEL_1);
HAL_TIM_IC_Stop_IT(htim,TIM_CHANNEL_1);
capture_cnt++;
break;
default:
break;
}
}
}
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
test = 1;
if (hadc->Instance == ADC1)
{
max_value = ADC_Value[0];
min_value = ADC_Value[0];
for (int i = 0; i < 4095; i++)
{
if (ADC_Value[i] > max_value)
{
max_value = ADC_Value[i];
}
if (ADC_Value[i] < min_value)
{
min_value = ADC_Value[i];
}
}
ADC_MaxValue = ((float)max_value * 3.3f) / 4095.0f;
ADC_MinValue = ((float)min_value * 3.3f) / 4095.0f;
processFFT();
if (m >= 1000000)
{
m = 10000; // Reset frequency to 10 kHz
check = 0;
}
HAL_ADC_Stop_DMA(&hadc1);
lastTick = HAL_GetTick();
adc_conversion_complete = 1;
}
}Solved! Go to Solution.
2024-10-23 1:26 AM
Well, try a whole range of input voltages.
JW
2024-10-23 9:05 AM
Hello, thank you for your assistance. I have resolved the issue. I found that the problem was with the development board. After purchasing a new one, the problem was solved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.