2025-12-11 1:15 AM
Hi fellows,
I have a custom board with STM32F407VGT6. The board was able to be programmed via the JTAG (4 wire JTAG interface; Boot pin is pulled low to ground and reset is connected to the JTAG interface (Nrset pin)) with a segger programmer - multiple times at that and can run for hours, however sometimes it code wipes.
The board works fine for some time, but only upon boot-up (at random, happened twice thus far) we have seemingly a code-wipe as well as a bricked chip with the RDP set to 0xFF and unable to do anything with the chip. This does not happen during continuous running of the chip.
We have this across 2 differently designed boards, which are designed according to the reference manual for power supply and for the tests were supplied with external linear regulator with low noise.
I have seen some posts here but not conclusive solutions or cause for this issue, is it possible to trigger this externally via hardware faults ?
The chip reports back correctly via the STM32Cube Programmer (V2.18) but unable to download or erase flash as option bytes can't be read and report as 0xFF.
Does anyone have ideas or explanations for this behaviour ?
2025-12-16 6:46 AM
> could this be caused by ESD issues ?
That's always a possibility, and it is not always destructive.
But the way I'm handling the "naked" boards on my desk here (custom PCBs, Nucleos - kinda first EMI test by developer sloppiness ... :D), either PCB layout must be really bad or / and you have some strong EMI sources nearby.
Have you tried putting the PCB into a case?
2025-12-16 6:52 AM
An airport radar or eye level, about 200m distance from where the boards are tested might count as strong EMI source, not sure though.... :D
I would not expect the flash to corrupt or anything else with ESD, at least the flash...
2025-12-16 10:46 PM
>... Boot pin is pulled low to ground and reset is connected to the JTAG interface (Nrset pin)) with a segger programmer - multiple times at that and can run for hours, however sometimes it code wipes.
>...The board works fine for some time, but only upon boot-up (at random, happened twice thus far) we have seemingly a code-wipe as well as a bricked chip with the RDP set to 0xFF and unable to do anything with the chip. This does not happen during continuous running of the chip.
A few weeks ago I had a somewhat similiar problem with a Raspberry Pi Zero.
It booted up fine, and I could login via ssh.
However, a few minutes after running apt update / apt upgrade, the connection was lost and the board unresponsive.
Not only that, the SD card was irretrievably corrupted.
As it turned out, the power supply was only marginally sufficient.
It was ok under lght loads, but under higher stress, the supply fell below the brown-out level, and the system crashed.
I would highly recommend to investigate and check the power supply rails, perhaps compare yours with reference designs. I'm not a hardware developer, I would add.
> An airport radar or eye level, about 200m distance from where the boards are tested might count as strong EMI source, ...
Not sure what you mean with "eye level".
But an airport radar is unlikely the cause, this is usually directed radiation, pointing upwards.
If your location is hit by the direct beam from 200m, you will have much more serious problems than just crashing STM32F407 boards ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.