2019-05-15 4:11 AM
I'm using SPI Protocol in two STM32F407ZGT6 , one master and one slave
Board has 3.3v LDO regulator and Input Voltage has 5v
When power supply connected SPI program correctly work but in this case when disconnect SPI wires and connect again we face of overheating and ic damaged
I read about hot swapping ( replacing or adding components without stopping or shutting down the system ) in the web but can't find any resource in STM32 MCU
2019-05-15 4:53 AM
The techniques aren't exactly STM32 specific.
2019-05-15 12:26 PM
"overheating and ic damaged" is normally a sign of pin voltages above maximum ratings. Review your schematic, wiring and setup/
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.