2013-12-05 3:17 AM
Hey there,
Our problem is that we get random faults (memory, bus or usage)! The handlers are calling sporadically between 10s to some hours! But we have also pcb�s without any issues! We are using a custom environment with a STM32F405ZGT and an external PSRAM! From software side we have the Keil os without micro lib (due to usage of a cpp library) We are using excessive dynamic memory but only in external RAM! All other RAM access goes to internal one. A further interface we are using in a high priority is the SPI2 interface with DMA functionality! If we stop in an error handler, we recognize invalid addresses in pc (like: 0xE0C001E0; 0x804AED2; 0xFFFFFFFE; 0x46604630 or 0x00000000) Does anybody have an idea? #stm32f4 #stm32 #fault2013-12-06 5:41 AM
Hi,
I work with sebbo at this issue! Actual I've 6 pcb's with 130MHz running! Since 12 o'clock I've no issue on it. (I let it run for some more hours to ensure the statement) Then I've 4 pcb'swith 168MHz system clock and I've slow down every FSMC clock parameter by 1 HCLK! In this case I got the errors
! I'm also confused if it is a HW or SW issue!?2013-12-06 5:51 AM
Another point of view is that we have pcb’s, those are running at 21 degree’s with no issues but at -10 degree they crash’s !
We also do tests with some capacities (33pF) at the control lines to the RAM…that shifts the issue a little bit!
The issue is coming no more often…but that could not a solution for the issues!
I believe the capacities and the temperature are shifting the timing a little bit!2013-12-06 6:21 AM
Do you set the FSMC pins' speed at 100MHz?
Do you switch on the compensation cell? [EDIT] have looked into grounding and decoupling issues at and around the mcu and PSRAM (i.e. experimenting with ground ''enforced'' by external wires, adding small ceramic capacitors as close to supply pins as possible) JW2013-12-09 1:03 AM
Hi Jan,
>Do you set the FSMC pins' speed at 100MHz? yes we setup the speed to 100MHz! >Do you switch on the compensation cell? No...we had not switched on this compensation! In the morning I've switched on the CMP_PD bit and the issue is much more rarely! It looks much better... >experimenting with ground ''enforced'' by external wires, adding small ceramic >capacitors as close to supply pins as possible) we did much such things but with no success. But maybe it is a combination of many little things!? Sabbo is testing the CCM memory...we are not using before! That was also a good hint from clive! Sabbo is getting some ''memory manage faults'' after a short while, if the stacks are running in the CCM memory! As third we try to get running the trace lines for postmortem analysis!2013-12-09 4:16 AM
How about looking at the external bus with a logic analyzer, and triggering on the faults?
CCM won't support DMA, but is a good place for stacks and variables.External Memory has significantly lower bandwidth than internal RAM, where possible DMA into internal RAM, there will be less/shorter contention.2013-12-09 8:31 AM
>CCM won't support DMA, but is a good place for stacks and variables.
yes...we've shifted the stacks to CCM, but the issue is still alive! >External Memory has significantly lower bandwidth than internal RAM, where possible >DMA into internal RAM, there will be less/shorter contention. the external RAM is already used from heap only... (actual we don't get our Ulink pro to run with the trace option!? What is the best way: 4 wire ETM trace? We got ''Data Stream Error'' after some seconds!) >How about looking at the external bus with a logic analyzer, and triggering on the faults? I think that's not an option for us we have no experience with that.2013-12-09 8:40 AM
>How about looking at the external bus with a logic analyzer, and triggering on the faults?
I think that's not an option for us we have no experience with that.
Unfortunately if you have a timing issue this might represent the most effective way to nail it down. If you can't rent or attach an analyzer consider a multi-channel scope looking at the control signals, and validating the device timing against the specs for the external memory? The processor trace may tell you how you arrived at a particular event, as would adequate telemetry, but external bus activity and DMA may not be apparent. ie Initiation of a DMA transfer, or multiple active transfers, etc. Consider derating the settings for the external memory, and reducing the SPI bandwidth.
2013-12-13 3:17 AM
2013-12-14 5:18 AM
The part doesn't use multiplexing (ie where address and data lines share pins at different phases during access)
SRAM or PSRAM configurations should be appropriate.What's the current configuration look like? 70 ns timing?What does the memtest code look like? This should really be able to catch failures if done aggressively. Is it done in assembler? Does it write random patterns?2013-12-16 12:18 AM
Thats our basic configuration:
p.FSMC_AddressSetupTime = 0x4;// (1/168MHz) * 4 -> 23,8ns p.FSMC_AddressHoldTime = 0x4;// (1/168MHz) * 4 -> 23,8ns p.FSMC_DataSetupTime = 0x04;// (1/168MHz) * 4 -> 23,8ns p.FSMC_BusTurnAroundDuration = 0x0;// no HCLK cycles added p.FSMC_CLKDivision = 0x1;// clock divided by 2 p.FSMC_DataLatency = 0x2;// 1/(168MHz/(FSMC_CLKDivision+1)) * (2+2) -> 47,6ns p.FSMC_AccessMode = FSMC_AccessMode_A; FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM1; FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Enable; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_PSRAM; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b; FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable; FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Enable; FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &p; FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &p; Then I test with p.FSMC_AddressSetupTime = 0xB;// (1/168MHz) * 12 ->70,8ns p.FSMC_AddressHoldTime = 0xB;// (1/168MHz) * 12 -> 70,8ns p.FSMC_DataSetupTime = 0x0B;// (1/168MHz) * 12 -> 70,8ns p.FSMC_BusTurnAroundDuration = 0x0;// no HCLK cycles added p.FSMC_CLKDivision = 0x1;// clock divided by 2 p.FSMC_DataLatency = 0x0; p.FSMC_AccessMode = FSMC_AccessMode_A; FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; In both configurations we have the issue!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.