2014-01-03 6:25 AM
2014-01-04 3:41 AM
i have a nasty / tricky / stinky solution..
on flag TXI :.... bla bla
if (I2C_GetITStatus(I2C1, I2C_IT_TXIS)) { jTX++; I2C_ClearITPendingBit(I2C1, I2C_IT_TXI); if (jTX > 2) { // without this delay below, the byte sent previously was gone !! uint16_t delay; for (delay = 0; delay < 0x100; delay++) {} // brutally kill I2C device and ressurect it // maybe not so nasty/stinky because it only // needed to be done once, after MCU's resetted I2C_Cmd(I2C1,DISABLE); I2C_Cmd(I2C1,ENABLE); } else I2C_SendData(I2C1,jTX); return 0; } is it a solution .. or not ? please advice... update : it is not a solution. after killing I2C and ressurect it, the I2C becomes screwed !!2014-01-04 6:38 AM
You have make a very comprehensive presentation, I'm not much into the F0, CooCox, or I2C, so I'm not sure I can give much advice in those regards.
2014-01-04 7:17 AM
i'm really very glad to see you in my thread, clive1
i just need a very little advice/info .. : => usually we send something using I2C_SendData(I2Cx, Data) in order to suppress TXI interruption.... my question is : how to CLEAR the TXI flag (Transmit Interrupt) without sending something .. !! ?? !!2014-01-06 4:34 AM
RM0091, Rev4, 24.7.7 (I2Cx_ISR), Bit 1 TXIS: Transmit interrupt status (transmitters)
[...] Note: This bit is cleared by hardware when PE=0. JW2014-01-06 8:13 AM
From: waclawek.jan
Posted: Monday, January 06, 2014 1:34 PM
Subject: STM32F030F4P6 I2C Slave Transmitter Problem : TXI event triggered more times than requested by I2C master
RM0091, Rev4, 24.7.7 (I2Cx_ISR), Bit 1 TXIS: Transmit interrupt status (transmitters)
[...] Note: This bit is cleared by hardware when PE=0.
JW
thanks JW for your Reply but still no luck... I tried it with this : I2C1->ISR &= (uint32_t)0xFFFFFFFD; CMIIW ...
Clear PE flag (Bit 0 of I2C1->CR1 is exactly the same with
I2C_Cmd(I2C1,DISABLE);
(already in my ''nasty'' solution)
Others ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.