2017-11-23 8:30 AM
Hi all,
CubeMX v4.23.0
CubeF3 fw package v1.18.0
I'm finding that a clean newly created project & created source does not enable the SysTick timer.
The project is a mix of LL and HAL.
I have to add
HAL_ResumeTick() to get it running.
An example:
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init *//* USER CODE END Init *//* Configure the system clock */ SystemClock_Config();/* USER CODE BEGIN SysInit */ HAL_ResumeTick(); /* USER CODE END SysInit *//* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM1_Init(); MX_TIM2_Init(); MX_TIM3_Init(); MX_TIM4_Init(); MX_USART1_UART_Init(); MX_USART2_UART_Init(); MX_USB_DEVICE_Init();#systick #stm32f401
2017-12-04 7:23 AM
Hi
Williams.Mark
,This issue is reported internally for check.
-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.