2017-11-22 3:57 AM
Hi,
I have problems with ethernet (using the HAL library 1.8.0) on the STM32F756ZG.
If I place the DMA buffers in the DTCM (0x20000000-0x2000ffff), it works fine. If I place the DMA buffer anywhere else (SRAM1, SRAM2), I get only on every second ping an answer (50% loss).
I don't use the MPU and I don't activate the data cache (SCB.CCR.DC = 0).
I also tried (despite the dcache being deactivated) flushing the data cache (SCB_DCacheClean()) before sending data in low_level_output() and invalidating the data cache (SCB_DCacheInvalidate()) before reading data in low_level_input(), but to no avail.
Does anybody has an idea?
TIA,
diz
2017-11-22 4:01 AM
Oops, misspelled the cache control calls, meant SCB_InvalideatDCache() and SCB_CleanDCache().
2017-11-30 1:23 AM
Really no one has an idea? Will move on to STM32F765 due to other reason anyway -- will be interesting to see if the same occurs on this MCU.
2017-12-04 7:22 AM
My problem was solved by
https://community.st.com/0D50X00009XkgffSAB
, i.e. I added __DSB() to HAL_ETH_TransmitFrame() as suggested by daniel nielsson.After changing to STM32F765 that fix no longer seems to be necessary.
STM32F765 is r1p0, STM32F756 is r0p1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.