2016-02-25 9:23 PM
Hello,
I have looked through the app note AN4365, and I have a question about SLEEP mode that isn't clear in the document. The chart on Page 8 doesn't really disambiguate which one of those is sleep mode. So I am interested to find out this: if I want to SLEEP the device, yet still run a timer interrupt, what is the actual current in uA/MHz? I'm planning on running the SystemCoreClock at 84Mhz. Thanks!2016-02-26 7:23 AM
Hi roofie01,
In figure 2 of AN4365, we have chosen to put one mode from dynamic power modes ( Run and sleep) which is Run mode with all static power mode ( Stop, standby , Vbat).
So to figure out the uA/Mhz ratio of sleep mode, you need to check the related datasheet in ''Typical and maximum current consumption in Sleep mode'' table where you find the power consumption per frequency. You consider the typical value of ''All peripherals disabled''.-> for example : in STM32F401 datasheet at this link , in Table 26 , you find that the current consumption in sleep mode; All peripherals disabled, is like the following:[@84 MHz: current consumption is 5, 3 mA] -> 5,3/84 = 63 uA/MhzAfter that, if you need to make real estimation about you consumption at sleep mode, you have to add the current consumption of the enabled peripherals in your application (ex. Timer), from 'Peripheral current consumption '' Table 33.-Hannibal-
2016-02-29 7:03 AM
Very helpful reply, thanks for good clarity!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.