2016-08-23 7:25 AM
Hello there,
In STM32F4 I am interfacing with a hall sensor attached to a BLDC motor. I have successfully configured TIM4 as HALL/ XOR inputs timer. The problem is, I am having a bit of a problem with interpreting how to use this mechanism with a BLDC motor. My observations are: - CNT register works as regular, it increases/ decreases (depending on the config) with the prescaller and period config. - As soon as I move the motor shaft and the 3 hall outputs change its state, the actual CNT value is copied to the CCR1 register and CNT itself is reset. If my observations are correct, the CCR1 register gives a somewhat accurate information about motor speed. I kind of expected something else- What I need is the information what is the exact hall output state from 1 to 6). I could get that info simply by pooling the 3 inputs state, or using interrupts. But I thought that the Hall timer mechanism gives some better aid in this. So should I just check the lines state each time I get an interrupt from CNT = 0? Or am I not getting something here. I would appreciate all help.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.