STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can bus not receiving any messages from PCAN

Posted on January 08, 2015 at 12:06Ich benutze STM32 Cube HAL driver auf STM32F429 f�r CAN bus communication zwischen Microcontroller und PCAN View.Ich kann sendet die Nachricten zu PCAn aber kann ich nicht empfangt jedes nachrichten von PCAN.Meine ...

rm239955 by Associate II
  • 2749 Views
  • 7 replies
  • 0 kudos

Timer 15 encoder mode !

Posted on August 23, 2016 at 22:41Yeah well I'm going to say that even though the input sections of timer 15 *seem* to have the necessary signaling input conditioning (xor)  so it could be used as a quadrature encoder signal interface, it seems odd ...

STM32F411E-DISCO board basics

Posted on August 21, 2016 at 10:36I was wondering if anyone is able to provide the following: - A link to the prebuilt existing image as originally supplied with the STM32F411E discovery boards. Preferably as a single file, but failing that clear di...

Help with alternate function routing

Posted on August 24, 2016 at 05:43I have a STM32F401re Nucleo board + Segger.edu J-Link. I am monitoring I2C signals using an Intronix LogicPort serial bus decoder. The development system is Rowley-Crossworks (v3.6.5.2016061400.2836 :) for ARM, whic...

troneeee by Associate II
  • 1196 Views
  • 1 replies
  • 0 kudos

stm32f3xx SPI read failure

Posted on August 24, 2016 at 01:18GreetingsUsing the HAL function  HAL_SPI_TransmitReceive()  to read erased data (i.e. all FF's) data from an external serial NOR device  I get a block of 0's at either the start or the end of a 256 byte read. Using ...

Assert_param problem

Posted on August 23, 2016 at 21:23Hello all,I'm a begineer with the ARM Discovery kit (STM32F4) and I'm trying to compile a test program when I try to compile it, an error appears : no definition for ''assert_param''. What I can do ? where does the ...

glias37 by Associate
  • 947 Views
  • 1 replies
  • 0 kudos

STM32F4 Hall sensor output interpretation

Posted on August 23, 2016 at 16:25Hello there, In STM32F4 I am interfacing with a hall sensor attached to a BLDC motor. I have successfully configured TIM4 as HALL/ XOR inputs timer. The problem is, I am having a bit of a problem with interpreting h...

_

Posted on August 23, 2016 at 15:17 Thankyou for the additional pointers, this has given me some things to check out. It might take some time to get through it all but I hope to be able to do so soon. I'll write up a more detailed reply once I've man...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.