2015-02-08 7:16 PM
Hi all,
I was able to use the code below to init the SPI and read the values fromaccelerometerSPI_InitTypeDef SPI_InitTypeDefStruct;
GPIO_InitTypeDef GPIO_InitTypeDefStruct;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE , ENABLE);
SPI_InitTypeDefStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitTypeDefStruct.SPI_Mode = SPI_Mode_Master;
SPI_InitTypeDefStruct.SPI_DataSize = SPI_DataSize_8b;
SPI_InitTypeDefStruct.SPI_CPOL = SPI_CPOL_High;
SPI_InitTypeDefStruct.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitTypeDefStruct.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set;
SPI_InitTypeDefStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256;
//seems like it was here causing trouble
SPI_InitTypeDefStruct.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_Init(SPI1, &SPI_InitTypeDefStruct);
GPIO_InitTypeDefStruct.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_7 | GPIO_Pin_6;
GPIO_InitTypeDefStruct.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitTypeDefStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitTypeDefStruct.GPIO_OType = GPIO_OType_PP;
GPIO_InitTypeDefStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitTypeDefStruct);
GPIO_InitTypeDefStruct.GPIO_Pin = GPIO_Pin_3;
GPIO_InitTypeDefStruct.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitTypeDefStruct.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitTypeDefStruct.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitTypeDefStruct.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOE, &GPIO_InitTypeDefStruct);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_SPI1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_SPI1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_SPI1);
GPIO_SetBits(GPIOE, GPIO_Pin_3);
SPI_Cmd(SPI1, ENABLE);
SPI_send(0x23, 0xc9);
// resetting the accelerometer internal circuit
//SPI_send(0x20, 0x67); // 100Hz data update rate, block data update disable, x/y/z enabled
SPI_send(0x20, 0x97);
//SPI_send(0x24, 0x20); // Anti aliasing filter bandwidth 800Hz, 16G (very sensitive), no self-test, 4-wire interface
SPI_send(0x24, 0x00);
// Anti aliasing filter bandwidth 800Hz, 2G ( sensitive ??), no self-test, 4-wire interface
SPI_send(0x10, 0x00);
// Output(X) = Measurement(X) - OFFSET(X) * 32;
SPI_send(0x11, 0x00);
// Output(Y) = Measurement(Y) - OFFSET(Y) * 32;
SPI_send(0x12, 0x00);
// Output(Z) = Measurement(Z) - OFFSET(Z) * 32;
void
SPI_send(uint8_t address, uint8_t data)
{
GPIO_ResetBits(GPIOE, GPIO_Pin_3);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, address);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
SPI_I2S_ReceiveData(SPI1);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, data);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
SPI_I2S_ReceiveData(SPI1);
GPIO_SetBits(GPIOE, GPIO_Pin_3);
}
uint8_t SPI_read(uint8_t address)
{
GPIO_ResetBits(GPIOE, GPIO_Pin_3);
address = 0x80 | address;
// 0b10 - reading and clearing status
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, address);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
SPI_I2S_ReceiveData(SPI1);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
SPI_I2S_SendData(SPI1, 0x00);
while
(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE) == RESET);
GPIO_SetBits(GPIOE, GPIO_Pin_3);
return
SPI_I2S_ReceiveData(SPI1);
}
Then I combined these code with my project which has an 500Hz interrupt.
It always work at first but if i unplug the board then plug it in again, SPI will only read zeros, even though theLIS3DSH still have readings(i usedoscilloscope checked it). I had to download the shorter version of the project code( taking out most of the code in the interrupt) to get SPI to work properly again.
I am using the
Kickstart, size-limitedIAR ewarm I thought it was because my code exceed the limit. But I did not get warning and my code was not more than 32kb.
I am just confused since it works until I unplug it. Could someone give me some suggestions?
Thanks
#!stm32f4-disco #stm32f4 #discovery #spi #device
2015-02-09 2:20 PM
I decided just to add the SPI_DeInit(...) before SPI_Init(...). This seems to solve the problem. I still dont understand why it wont reset itself though. Could someone explain this? Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.