2017-11-07 2:41 PM
Hello,
I am trying to run a custom example of USART6 transmitter from the STM32F4 Discovery (so using an STM32F407VGT) and I am having problems since I only see garbage characters like '�' through the PC serial console (Putty or screen).The source code I am testing is the following one:
#include <stm32f4xx.h>
volatile uint8_t flag;
void EXTI0_IRQHandler(void)
{
//USART_SendData(USART6, 0xaa);
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
// keep the ISR as short as possible
// set the flag and go out
USART_SendData(USART6, 0x41);
EXTI_ClearITPendingBit(EXTI_Line0);
}
}
int main(void)
{
// GPIO, NVIC and EXTI declarations
GPIO_InitTypeDef gpio_t;
USART_InitTypeDef usart_t;
//USART_ClockInitTypeDef usart_clk_t;
NVIC_InitTypeDef nvic_t;
EXTI_InitTypeDef exti_t;
RCC_DeInit();
// Enable resonator frequency
RCC_HSEConfig(RCC_HSE_ON);
while (!RCC_WaitForHSEStartUp())
;
//RCC_PLLCmd(DISABLE);
//RCC_PLLConfig(uint32_t RCC_PLLSource, uint32_t PLLM, uint32_t PLLN, uint32_t PLLP, uint32_t PLLQ)
RCC_PLLConfig(RCC_PLLSource_HSE, 4, 50, 2, 1);
RCC_PLLCmd(ENABLE);
while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) != SET)
;
// Configure AHBP Clock
RCC_HCLKConfig(RCC_SYSCLK_Div1);
// set APB2 clock divider (PPRE2 bits)
RCC_PCLK2Config(RCC_HCLK_Div2);
// Sys clock config is the PLL
RCC_SYSCLKConfig(RCC_SYSCLKSource_HSE);
//RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
SystemCoreClockUpdate();
// Enable SYSCFG and USART6 Clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG | RCC_APB2Periph_USART6, ENABLE);
// Enable GPIOA and GPIOC Clock
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOC, ENABLE);
// configure GPIOA_0 as input
gpio_t.GPIO_Pin = GPIO_Pin_0;
gpio_t.GPIO_Mode = GPIO_Mode_IN;
//gpio_t.GPIO_OType = GPIO_OType_PP;
gpio_t.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOA, &gpio_t);
// configure GPIOC_6 to AF USART6 Tx
// Configure port as pushpull, 50MHz and No pull up & down
//gpio_t.GPIO_OType = GPIO_OType_PP;
//gpio_t.GPIO_PuPd = GPIO_PuPd_NOPULL;
//gpio_t.GPIO_Speed = GPIO_Speed_2MHz;
// Configure PC6 as alternate function
gpio_t.GPIO_Pin = GPIO_Pin_6;
gpio_t.GPIO_Mode = GPIO_Mode_AF;
GPIO_Init(GPIOC, &gpio_t);
// Configure PC7 as alternate function
gpio_t.GPIO_Pin = GPIO_Pin_7;
gpio_t.GPIO_Mode = GPIO_Mode_AF;
GPIO_Init(GPIOC, &gpio_t);
/* Connect PC6 to USART6_Tx*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);
/* Connect PC7 to USART6_Rx*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6);
usart_t.USART_BaudRate = 115200;
usart_t.USART_WordLength = USART_WordLength_8b;
usart_t.USART_StopBits = USART_StopBits_1;
//usart_t.USART_Parity = USART_Parity_No;
usart_t.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
usart_t.USART_Mode = USART_Mode_Tx | USART_Mode_Rx;
USART_Init(USART6, &usart_t);
USART_Cmd(USART6, ENABLE);
// Configure external interrupt for PA0
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);
exti_t.EXTI_Line = EXTI_Line0;
exti_t.EXTI_Mode = EXTI_Mode_Interrupt;
exti_t.EXTI_Trigger = EXTI_Trigger_Rising;
exti_t.EXTI_LineCmd = ENABLE;
EXTI_Init(&exti_t);
// enable EXTI0 interrupt for NVIC
nvic_t.NVIC_IRQChannel = EXTI0_IRQn;
nvic_t.NVIC_IRQChannelPreemptionPriority = 0;
nvic_t.NVIC_IRQChannelSubPriority = 0;
nvic_t.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&nvic_t);
flag = 1;
while(1)
{
if(flag)
{
USART_SendData(USART6, 0x01);
}
}
return 0;
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Even if the serial console configuration matches the USART configuration, I cannot receive the correct character.
Digital logic (both Tx and Rx side) is all working at 3V3, so the voltage threshold are OK.The USART configuration is copied from the USART_HyperTerminal example of Standard Peripheral Libraries.
What's wrong or what more configuration I am missing in my code ? Thank you in advance.Regards,
Simon
Solved! Go to Solution.
2017-11-08 7:52 AM
Solved !
The problem was in the definition of HSE into stm32f4xx.h.
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t) 8000000) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */�?�?�?�?�?�?
It is defined to 25 MHz. I changed to 8 MHz (since I am using this resonator value) as above and now everything works fine.
Simon
2017-11-08 2:31 AM
One strange thing I noticed, is that if I comment the settings for PC7 (AF USART6_TX) so commenting these lines:
// Configure PC7 as alternate function
gpio_t.GPIO_Mode = GPIO_Mode_AF;
gpio_t.GPIO_Pin = GPIO_Pin_7;
GPIO_Init(GPIOC, &gpio_t);�?�?�?�?�?�?�?�?
the transmitter doesn't work.
If the USART is configured in TX mode only, the RX pin should be free to be used for other purposes. Shouldn't it ?
I suspect that the gcc compiler is not generating good code..
Simon
2017-11-08 3:08 AM
I only see garbage characters like '�' through the PC serial console
That usually means that the baud rate is wrong.
Have you checked what is actually happening on the pin - with an oscilloscope or logic analyser ?
2017-11-08 4:33 AM
Hello
Neil.Andrew
,Andrew Neil wrote:
That usually means that the baud rate is wrong.
This is what I also suspect, but I am not totally sure about it.
Yes I do have an oscilloscope and I can see the transmitted signal on PC6 pin (USART6_TX).
Unfortunately I don't have a logic analyzer.
Simon
2017-11-08 4:49 AM
So does your 'scope confirm that the signal is correct?
In particular, the board rate?
Polarity ... ?
2017-11-08 5:35 AM
Neil.Andrew
you are right. I could do better tests.Sending a just a bit (0x01) at 115200 bps the pulse width is 25 us with leads to a wrong baudrate.
To ensure myself, I compared the pulse width with a USB/232 cable sending the same data at 115200, and pulse width is approx 9 us, which is correct.
I confirm the baud-rate is wrong.
2017-11-08 7:52 AM
Solved !
The problem was in the definition of HSE into stm32f4xx.h.
#if !defined (HSE_VALUE)
#define HSE_VALUE ((uint32_t) 8000000) /*!< Value of the External oscillator in Hz */
#endif /* HSE_VALUE */�?�?�?�?�?�?
It is defined to 25 MHz. I changed to 8 MHz (since I am using this resonator value) as above and now everything works fine.
Simon
2017-11-08 11:04 AM
Hmm ... I guess someone thought they were being 'helpful' with that - but silently providing an arbitrary default like that is almost certainly
not
helpful!!It would have been far more helpful to do something like:
#if !defined (HSE_VALUE)
#error 'HSE_VALUE must be definedasthe External oscillator frequency, in Hz'
#endif /* HSE_VALUE */
2017-11-08 11:06 AM
Note that an easier way to test serial comms is to continuously send 'U' - since that gives a nice ...1010101... pattern which is easy to see on a 'scope.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.