STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Seeking contractor for BlueNRG on an iPhone application

Posted on November 07, 2017 at 21:36We are looking for a contractor that can help develop the Bluetooth interface on a BlueNRG device that interfaces to an iPhone app. This is a paid position to someone with suitable experience. May include sponsore...

VTOR description error, ST Cortex-M7 manual

Posted on November 08, 2017 at 23:58The description of the VTOR register is incorrect in the ST Cortex-M7 programming manual (PM0253). The description ST Cortex-M4 programming manual (PM0214) is correct. The description in the ARM ARMv7-M Architectu...

dbrown by Associate II
  • 3227 Views
  • 2 replies
  • 1 kudos

STM32L496G-Discovery PSRAM problem

Posted on November 08, 2017 at 10:04Hey, I'm using STM32L496G-Discovery before our PCBA will arrive. According to the docs there is 8Mbit (1MB) PSRAM on board, but in ALL ST examples with the board just 64k of it defined into icf (from 0x1000000 to ...

SD Card breakout board

Posted on May 21, 2017 at 22:05hey guys,i'm interested in a SD breakout board for my STM32F427 disco board.I'd like to use the MCUs SDIO Pins for the communication with the SD breakout board.Of course when you search for 'sd breakoutboard' there are...

Resolved! 32F769IDISCOVERY UART7 usage

Posted on November 08, 2017 at 13:41I selected the 32F769IDISCOVERY board in CubeMX.Why is UART7 in CubeMX disabled?The pins in the conflicts list are not mapped or active.For my app I need the Arduino Pin D3 which is UART7_RX.I studied the schemati...

STM32F446 PA5 output levels at high frequency

Posted on April 25, 2016 at 10:36This is one for the ST insiders. On a Nucleo64 (SB21, SB29, SB44 all disconnected) with STM32F446, the PA5 pin has been configured as AF5 (SPI1_SCK/I2S1_CK), push-pull, OSPEEDR set to 0b11 (and later tried also 0b10)...

Trigger ADC1 scan using TIM1 CC1 on F410RB

Posted on September 20, 2016 at 13:08 Hi, I use STM32F410RB, and I need to trigger an ADC1 scan regular conversion every TIM1 CC1 event. I am sure that TIM1 works, because I have an interrupt that is triggered every CC1 event. I tried to ...

Resolved! STM32F4 and USART issues

Posted on November 07, 2017 at 23:41 Hello, I am trying to run a custom example of USART6 transmitter from the STM32F4 Discovery (so using an STM32F407VGT) and I am having problems since I only see garbage characters like '�' through the PC se...

simo zz by Senior II
  • 3893 Views
  • 8 replies
  • 0 kudos

Resolved! STM32F303 OCREFCLR with Comparator Output

Posted on November 08, 2017 at 14:28Hello Everyone,I have a question about STM32F303VCT6 MCU's Hardware Comparator Unit.I want to use 6 of the comparators as window comparator. I have no problem with this installation. But I also want to use this 3 ...

Cemre . by Associate II
  • 1871 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.