2021-05-26 10:49 PM
The RTC looses 15 min every 8 hour aprox when the main power is on. I have selected the LSE as the RTC clock, as i show in the images, and i have a 32.768 Khz 10 ppm crystal with a 9 pF load. I thought that maybe it was due to a bad match of the crystal capacitors but the RTC works fine when the main power is off! I really dont know what is going on... Thanks in advance.
Solved! Go to Solution.
2021-06-07 11:41 PM
In the end it really seems like a hardware problem. The MCO output is not stable when i turn on or off some peripherals...So i will try to be more careful with the RTC in the next design and see if the problem dissapears. Thanks for the help
2022-03-29 3:22 AM
Dear @DCajigal I have same problem. How did you solved this problem?
https://community.st.com/s/question/0D53W00001ScZorSAF/internal-rtc-clock-lag-issue
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.