2017-11-02 6:36 AM
Hi,
I'm facing a problem of getting the STM32F3 Discovery board bootloader to work. AN2606 calls for pattern 2 to be applied so I pulled up the BOOT0 pin. A check with STLink shows the nBOOT1 bit is 1 so upon powering up the board, the application firmware inside the MCU did not run. But when I send 0x7f through USART1, there is no response from the bootloader.
Anybody has any idea what I'm missing?
2017-11-02 8:14 AM
USART needs to connect to at CMOS serial levels, need to be using Even parity, ie 9600 8E1
The 0x7F is a single character, need to use something like RealTerm in Hex mode.
Really no idea from question how you've actually got this wired up or how data is applied and reviewed.
2017-11-03 2:06 AM
Hi,
Thanks for your reply. When you mentioned about wiring, I did another check and found out I had soldered the USART1 Tx to an adjacent pin instead of PA9. Correcting it returns an NACK now
For info, I'm using a FTDI USB to Uart bridge to interface with the
STM32F3 Discovery board. The Tx output of the Uart bridge is buffered and pulled up to the 3V source on the Discovery board. I then used a Windows Terminal App to do the communications.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.