STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPTIM interrupt

Posted on November 02, 2017 at 10:08Is it possible to set LPTIM to have interrupt every ms?I did try some examples, and got PWM working with LPTIM on PB2.I can do that with TIM2, but then I got problem with system wake up, and I do not want that...

Resolved! STM32L4xx: standby and run mode

Posted on November 03, 2017 at 14:07Hallo, Since I think that the use of auto generated code using MXcube helps a lot, I have a question regarding the best workflow to use in the following case.My board is powered by an external power source. In thi...

stm32f769 VDD12DSI pin

Posted on November 03, 2017 at 10:36Hello, I am using stm32f769 bga package. We accidentaly connect VDD12DSI pin to VCAPSDSI pin and connect them to 3.3V VDD. We only gave power to the circuit for a few seconds. Could it damage the MCU? And if I dis...

halil by Associate
  • 1239 Views
  • 1 replies
  • 0 kudos

STM32F3 Discovery Bootloader No NACK Received

Posted on November 02, 2017 at 14:36Hi,I'm facing a problem of getting the STM32F3 Discovery board bootloader to work. AN2606 calls for pattern 2 to be applied so I pulled up the BOOT0 pin. A check with STLink shows the nBOOT1 bit is 1 so upon power...

Fong WH by Associate
  • 1349 Views
  • 2 replies
  • 0 kudos

uClinux

Posted on November 03, 2017 at 08:51HiI'm using a stm32f103ve development board and i want to run linux on it.I confront a version of linux named uClinux that is compatible with my board.ST has a pdf named AN3012 that describes the procedure of runn...

Ethernet issue (STM32F765BIT )

Posted on November 03, 2017 at 08:24Hello .,I am working on STM32 MCU in our custom board, In this I am facing some issues related to Ethernet interface. I manage to generate Ethernet code using STM cube MX,(Using in RMII), The code is working but n...

MANISH by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

Frequency capture in STM32F7

Posted on October 30, 2017 at 13:15I am working with STM32F765BIT MCU in our custom board, In that I need to measure some external signal frequency.I am using timer in input capture mode to measure the frequency. I have taken some reference example ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.