2012-09-24 3:36 PM
When I use DMA on the transmit SPI2 chanel (STM32F205) I consistently get FIFO errors at the end of the transfer, even though the FIFO is disabled. I verified the DMDIS flag is 0 in the DMA_SxFCR register but the DMA_HISR register still shows FEIF4 flag set. DMA stream 4 is configured as a dummy SPI clock, no memory or peripheral increment. Memory and peripheral burst is set to singular (byte). FIFO is disabled, threshold set to 1/4.
From what I read in the reference manual it should not be possible to get a FIFO error if the FIFO is disabled, yet it still happens. It doesn't affect transfers but is a mystery. Has anyone encountered the same situation? Jack Peacock #spi-dma-fifo2014-05-13 7:08 AM
Dear Jack,
Have you ever found a solution to this? I'm have the exact same scenario / behaviour as you, but on a STM32F207.Mario2014-05-13 11:48 PM
This is considered normal. Simply ignore the FIFO error, if you use Direct mode.
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DMA+and+Direct+Mode&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=146 JW2014-06-11 6:30 AM
Hi Mario,
Are you enabling the used peripheral before the corresponding DMA stream? If it is the case, a ''FEIF'' may be set. (please refer to AN4031/p32: Using the STM32F2 and STM32F4 DMA controller for more details). -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-06-11 6:55 AM
What the reference manual doesn't make clear is the FIFO error is also triggered by falling below the FIFO threshold.
Jack PeacockWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.