2014-05-07 1:42 AM
Hi,
I've a problem with my STM32F217VG. I need to use fat filesystem on MicroSD card (2 GB) to read/write/create files.I tried to use Chan FatFs module but it didn't working at all ...I use SD card in SDIO mode.When I debug: I call the sub ''f_mount'' and return an error! I follow the problem inside : ''disk_initialize'' >> ''SD_Init'' >> ''SD_PowerON'' >> ''CmdResp3Error'' return always ''SD_CMD_RSP_TIMEOUT'' ... with or without MicroSD !!!! I'm desperate :-(((1. I don't know if the subs ''SD_Init'', ''SD_PowerON''... are the right ones! Where I can find the correct sub for my STM32F217 ?2. What could be the problem ?Thanks. #stm32 #sdio-fatfs2014-05-07 3:08 AM
Did you checked that SDcard is connected to the MCU using the same pins that are configured in the software ?
2014-05-14 6:27 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.