STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 USART (overrun)

Posted on May 14, 2014 at 16:18 Hello, I am using USART 1 at 115200 and todayserious problems with USART overrun started to appear (yesterday everything was fine and I don't seem to remember any significant changes on this portion of the ...

oversc0re by Associate II
  • 3145 Views
  • 4 replies
  • 0 kudos

ACD1_In16 configuration

Posted on May 14, 2014 at 19:40I'm having some trouble configuring this ADC, I need to read the temperature of the internal sensor from the STM32F3 Discovery. But in order to do so I have to configure this particular ADC (ADC1_in16)

STM32 VDE self-test library for stdperiph_lib

Posted on May 08, 2014 at 09:28Dear ST; I want to Optimize my program,so for the safety,I need the self-test library.but I can not find it on the st.com,so I come here to get help from you guys. Thanks very much. Yours, liuwei #stm32f10x #stm32 #...

994724682 by Associate II
  • 3330 Views
  • 8 replies
  • 0 kudos

STM32F217VG + MicroSD + SDIO + FatFs problem

Posted on May 07, 2014 at 10:42Hi,I've a problem with my STM32F217VG. I need to use fat filesystem on MicroSD card (2 GB) to read/write/create files.I tried to use Chan FatFs module but it didn't working at all ...I use SD card in SDIO mode.When I d...

Open Source SW for AES Enc/Decr

Posted on May 14, 2014 at 07:12Hi,I'm looking for open source PC source to implement AES encryption decryption compatible with Crypto module in STM32F2. In other words I need to encrypt packets on PC side and decrypt them on STM side and vice verse....

dimax by Senior
  • 1010 Views
  • 1 replies
  • 0 kudos

Leaving Standby by WakeUp pin and RTC Alarm

Posted on February 17, 2012 at 17:37We use a strategy to wake up the STM32F103 from standby mode by means of the wakeup pin and/or from the RTC alarm. In our implementation it appears that the wakeup from the RTC alarm does occur when the wakeup pin...

kris2399 by Associate II
  • 6505 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.