2015-04-28 2:25 AM
SPI3 is configured as master readonly.
When the SPI is enabled then the clock can be monitored by an oscilloscope. The Interrupt-handler stops SPI3 after having received 3 bytes. However the data are always Zero regardless of MISO is 1 or 0.void SPI3_readonly_Config(void) { // SPI3 is Master readonly
/* available SPI3-Pins:
SPI3_SCK: PB3 (JTAG-conflict) use: PC10 SPI3_MISO PB4 (JTAG-conflict) use: PC11 SPI3_MOSI PB5 (JTAG-conflict) use: PC12, not used because readonly SPI3_NSS PA15, not used */ GPIO_InitTypeDef GPIO_InitStructure; SPI_InitTypeDef SPI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable the SPI clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE); /* Enable GPIOC clock, do not use MOSI and NSS */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);/* Connect SPI pins to AF6, do not use MOSI */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SPI3); /* SPI SCK pin configuration */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOC, &GPIO_InitStructure);/* SPI MOSI pin configuration not used, because readonly */
/* SPI MISO pin configuration as input */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_Init(GPIOC, &GPIO_InitStructure);/* NSS pin not used */
/* SPI configuration ----------------------------------------*/ SPI_I2S_DeInit(SPI3); SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_RxOnly; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low; SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 0; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_Init(SPI3, &SPI_InitStructure); /* Configure the SPI interrupt */NVIC_InitStructure.NVIC_IRQChannel = SPI3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable SPI_MASTER RXNE interrupt */ SPI_I2S_ITConfig(SPI3,SPI_I2S_IT_RXNE, ENABLE);// SPI_Cmd(SPI3, ENABLE); do not enable SPI here
}
uint8_t SPI3values[3]={0};
uint32_t SPIindex = 0;/* SPI3 Interrupt Handler */
void SPI3_IRQHandler(void) { // receive 3 bytes if (SPI_I2S_GetITStatus(SPI3, SPI_I2S_IT_RXNE) == SET) { SPI3values[SPIindex] = SPI3->DR; // content of array is always zeros if(SPIindex > 1) { /* disable SPI */ SPI3->CR1 &= 0xFFBF; // clear SPE Bit .... /* stop SPI, disable SPI clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, DISABLE); SPIindex = 0; } else SPIindex++; } }The clock configuration seems to be successful but what is wrong with the MISO-configuration?
2015-04-28 4:42 AM
The clock configuration seems to be successful but what is wrong with the MISO-configuration?
ALL the pins for the peripheral need to be in the GPIO AF Mode2015-04-28 5:20 AM
Yes, that makes sense. Now it works, thank you very much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.