2026-04-08 12:25 AM - last edited on 2026-04-08 3:51 AM by mƎALLEm
Post edited by a ST moderator to be inline with the community rules especially on the code sharing. In next time please use </> button to paste your code.
Hi
I am struggling getting context save restore working correctly, when operating the HASH hardware block using polling mode.
Basicly the flow is like this:
/* --- STEP 1: Start hashing first chunk --- */
HAL_HASHEx_SHA256_Start(&hhash, input1,strlen((char*)input1), digest,HAL_MAX_DELAY);
/* --- STEP 2: Save context --- */
HAL_HASH_ContextSaving(&hhash, context);
/* --- STEP 3: Restore context --- */
HAL_HASH_ContextRestoring(&hhash, context);
/* --- STEP 4: Continue hashing --- */
HAL_HASHEx_SHA256_Accumulate(&hhash, input2, strlen((char*)input2));
/* --- STEP 5: Finalize hash --- */
status = HAL_HASHEx_SHA256_Finish(&hhash, digest, HAL_MAX_DELAY);
However when calling HAL_HASH_ContextSaving the DINIS is not equal to 1 and CSRx registers return zeros as stated in the reference manual
How do it get the HW block in a state where i can do context swap when using polling mode.
Does any working example code for this use case exist ?
Best regards
Anders
2026-04-30 9:40 AM
Hello @aes2 ,
On STM32H5 HASH, there is a 17-word long FIFO that needs to be filled-up before the hashing process actually starts. 17 words, that means one block plus one additional 32-bit word
(please refer to RM0456, HASH chapter section 4.4 Message data feeding).
Only when the 17 words are written, then the flag DINIS goes to 1 and only then it is possible to save the HASH_CSR registers.
Here is a code extract I could find internally that may help
if (HAL_HASH_Init(&hhash2)!= HAL_OK)
{
Error_Handler();
}
/* The line below will trigger an automatic suspension as soon the first block is processed
and suspension conditions satisfied */
HAL_HASH_SwFeed_ProcessSuspend(&hhash2);
HAL_HASHEx_SHA256_Accmlt(&hhash2, (uint8_t *)sha256_tv_2, sizeof(sha256_tv_2));
if (HAL_HASH_GetState(&hhash2) != HAL_HASH_STATE_SUSPENDED)
{
Error_Handler();
}
HAL_HASH_ContextSaving(&hhash2, periph_status2);
/* Process sha256_tv_1 */
if (HAL_HASH_Init(&hhash1)!= HAL_OK)
{
Error_Handler();
}
HAL_HASHEx_SHA256_Accmlt(&hhash1, (uint8_t *)sha256_tv_1, 12);
HAL_HASHEx_SHA256_Accmlt_End(&hhash1, (uint8_t *)&sha256_tv_1[12], sizeof(sha256_tv_1) - 12, comp_digest_1, 0xffffffff);
/* Resume sha256_tv_2 processing */
HAL_HASH_ContextRestoring(&hhash2, periph_status2);
HAL_HASHEx_SHA256_Accmlt_End(&hhash2, (uint8_t *)&sha256_tv_2[64], sizeof(sha256_tv_2) - 64, comp_digest_2, 0xffffffff);
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.