2015-04-28 2:30 AM
Hi All:
I'm a newbie for the MCU programming. So far, I use SWD protocol to program STM32L151C6 chip with RDP level 1. I want to remove RDP level 1, program, and change level 0 to level 1. However, I follow the unlock steps of RM0038 reference manual to unlock the flash. First, I unlock the PECR register and option byte block. then I write the '0xFF5500AA' value into the address of flash 0x1FF80000 for setting RDP level 0, and write the '0xFF870078' value into the address 0x1FF80004 for set USE default values. Then, I unprotect the flash by writing 0xFFFF0000 into the address of option block from 0x1FF80008 to 0x1FF8001C After performing above steps, I find that the flash's FLASH_OBR doesn't show the RDP level 0 bits, 0x00F000AA. How can I to enable the RDP level 0 immedately after changing RDP level ? Regards ~We’re moving the ST Community to a new platform to give you a better and more reliable community experience.