2013-05-19 8:22 PM
Hi All,
I am a starter on STM32F207 MCU. My project is developing a system as a usb host device bridge. System architecture is: PC Host <----> F207 <----> usb flash drive F207 is similar as a ''usb bridge''. When F207 receive SCSI command from pc-host, it just resend to usb flash drive and do following thing(like read,write..etc). STMicro already provided usb_host_device_lib, it included a device example as SD card reader and a host example as reading/writing USB flash drive. I want to combine the two example that pc-host can enum,read, and write usb flash drive. Does anyone can provide example or give me some hint? Thank you very much.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.