2019-07-25 6:36 AM
Hello Guys
I am building a very simple application using CubeMX.
I am using two STM32F207ZG boards to communicate with each other over SPI bus without DMA or interrupts.
One is acting as a master another as as slave.
The slave settings are as follows.
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_4;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;The problem is i don't want to use NSS pin in hardware mode as it is being used for other purpose. If i configure NSS to be as software, i am missing one clock edge coming from the master and the slave is always stuck checking the TXE bit at the end of transmission inside HAL_SPI_TransmitReceive(....) function (because it is waiting for one more clock edge). i have verified it by sending 0xAA series from the master and the slave always receive 0x55.
/* Wait until TXE flag */
if(SPI_WaitFlagStateUntilTimeout(hspi, SPI_FLAG_TXE, SET, Timeout, tickstart) != HAL_OK)
{
errorcode = HAL_TIMEOUT;
goto error;
}But here if i reset the spi communication (i am resetting the controller), then surprisingly there after no problem in SPI communication.
Also if i put a CRO probe on the clock signal everything works fine.
I thought of capacitance issue but i have reduced the clock frequency to lowest possible but it didn't help, moreover i wonder if it would have been a problem with the capacitance why it would work after resetting the slave controller at the first place.
I would really appreciate if someone could please help me out of this issue.
Many thanks in advance. let me know if any other details are required
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.