2015-03-24 6:45 AM
Hello,
I want to sent some characters to a hyperterminal program. But my program wont work..I dont receive any characters in my hyperterminal. I am using the STM32-P107 development kit. The controller on it is the STM32F107VCI really need help here. I hope someone here see what i am doing wrong. I would really appreciate it. This is my code:/* Includes ------------------------------------------------------------------*/#include ''stm32f10x.h''#include ''stm32f10x_gpio.h''#include ''stm32f10x_rcc.h''#include ''stm32f10x_usart.h''#include <stdio.h>void USART_Print_Nick(void){ int i;//**************************************RCC Configuration*************************************\ /* Enable GPIO clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOC, ENABLE); /* Enable UART clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);//**************************************GPIO Configuration*************************************\ GPIO_InitTypeDef GPIO_InitStructure; /* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; // PA.02 USART1.TX GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART Rx as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; // PA.03 USART1.RX GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); //LED TOGGLE.. initialized // PA.08 = output port for LED GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure);//**************************************USART Configuration*************************************\ USART_InitTypeDef USART_InitStructure; USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USART2, &USART_InitStructure); /* Enable the USART2 */ USART_Cmd(USART2, ENABLE);//******************************************Program**********************************************\ while(1) { // 1010.1010 USART_SendData(USART2, 0xAA); //LED toggle GPIO_WriteBit(GPIOC, GPIO_Pin_8, 1); for(i=0;i<0x100000;i++); GPIO_WriteBit(GPIOC, GPIO_Pin_8, 0); for(i=0;i<0x100000;i++); }}2015-03-25 4:29 AM
Can you show us the code example that worked, perhaps that will shed some light on why this doesn't work.
2015-03-25 4:35 AM
Could it be that the board uses PD5/PD6 for USART2? That you need to use Bank D, and remap the USART2 there?
Last post,2015-03-25 5:11 AM
THanks for answer again!
No its connected to PA2 (tx) PA3 (rx), i checked again.I will show you but the software is really diffurrent and has other header / c files.I hope you can do something with this information. I still can't get it workThis is software with libraries from coocox. I think you can't do much with this.. I hope to hear it soon from you again //*****************************************************************************////! \file UartPrintf.c//! \brief Using UART0 to print some data to terminal.//! \version 1.0//! \date 6/29/2012//! \author CooCox//! \copy//!//! Copyright (c) 2009-2011 CooCox. All rights reserved.////*****************************************************************************#include ''xhw_types.h''#include ''xhw_ints.h''#include ''xhw_nvic.h''#include ''xhw_memmap.h''#include ''xdebug.h''#include ''xcore.h''#include ''xsysctl.h''#include ''xgpio.h''#include ''xuart.h''#include ''xhw_types.h''#include ''xhw_memmap.h''#include ''xhw_ints.h''#include ''xhw_nvic.h''#include ''xcore.h''#include ''xsysctl.h''#include ''xgpio.h''//*****************************************************************************////! \brief print some data to terminal.//!//! \param None//!//! \return None.////*****************************************************************************void UartPrintf(void){ unsigned long i; int y = 0xAA; int t; int d = 0x55; // //Set System Clock // xSysCtlClockSet(72000000, xSYSCTL_OSC_MAIN | xSYSCTL_XTAL_25MHZ); xSysCtlDelay(10000); xSysCtlPeripheralEnable(xSYSCTL_PERIPH_GPIOA); xSysCtlPeripheralEnable(xSYSCTL_PERIPH_GPIOD); xSysCtlPeripheralEnable(SYSCTL_PERIPH_AFIO); xSPinTypeUART(UART2TX,PD5); xSysCtlPeripheralReset(xSYSCTL_PERIPH_UART2); xSysCtlPeripheralEnable(xSYSCTL_PERIPH_UART2); xUARTConfigSet(USART2_BASE, 115200, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); xUARTEnable(USART2_BASE, (UART_BLOCK_UART | UART_BLOCK_TX | UART_BLOCK_RX)); // // Set GPIO port C pin 6 , 7 output mode. // xGPIODirModeSet( xGPIO_PORTC_BASE, xGPIO_PIN_6, xGPIO_DIR_MODE_OUT ); xGPIODirModeSet( xGPIO_PORTC_BASE, xGPIO_PIN_7, xGPIO_DIR_MODE_OUT ); // // Initionalize system clock. // xSysCtlPeripheralEnable( xSYSCTL_PERIPH_GPIOC ); while (1) { // Output low level. xGPIOPinWrite( xGPIO_PORTC_BASE, xGPIO_PIN_6 | xGPIO_PIN_7, 0 ); xUARTCharPut(USART2_BASE, y); for(i = 0; i < 1000000; i++); // Output high level. xGPIOPinWrite( xGPIO_PORTC_BASE, xGPIO_PIN_6 | xGPIO_PIN_7, 1 ); xUARTCharPut(USART2_BASE, d); for(i = 0; i < 1000000; i++); }}2015-03-25 5:18 AM
No its connected to PA2 (tx) PA3 (rx), i checked again.
Which version of the board? The most recent schematic definitely shows it using PD5/PD6 And in the code that works xSPinTypeUART(UART2TX,PD5); Try the code from the example I presented in the other thread.
2015-03-25 5:20 AM
https://www.olimex.com/Products/ARM/ST/STM32-P107/resources/STM32-P107_board_revision_C.pdf
2015-03-25 5:54 AM
Thanks a lot man!!
I had a old revision..I did remap the usart and it works! thanks a lot..!! Now i am gonna try receive etc!Thanks. Have a nice day man!!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.