2014-01-06 4:14 AM
Hi,
I would need 3 USARTs for a project (I am using stm32f103vct6 microcontroller). One USART is already functional properly which is USART1. I am trying same with USART2. Transmit is working fine but but RXNE flag is falsely setting up here and hence its giving garbage Rx character. I tried same code using arm-none-linux-gcc compiler in which its working fine (no false RXNE flag setting), hence i thought it could be compiler related issue. I am posting my code for reference.
void USART2_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; //enable bus clocks RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); //Set USART2 Tx (PA2) as AF push-pull GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); //Set USART2 Rx (PA3) as input floating GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_Init(USART2, &USART_InitStructure); //Enable USART2 USART_Cmd(USART2, ENABLE);}/* Usart functions --------------------------------- ------------------------*//******************************************************************************** Function Name : SerialPutChar* Description : Print a character on the HyperTerminal* Input : - c: The character to be printed* Output : None* Return : None*******************************************************************************/void SerialPutChar(u8 c){ USART_SendData(USART2, c); while (USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);}int GetChar (void){ while (USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); return USART_ReceiveData(USART2);}/******************************************************************************** Function Name : Serial_PutString* Description : Print a string on the HyperTerminal* Input : - s: The string to be printed* Output : None* Return : None*******************************************************************************/void Serial_PutString(u8 *s){ while (*s != '\0') { SerialPutChar(*s); s ++; }}void main(){ int data; USART1_Init(); Serial_PutString(''This is test put string function on open source compiler\r\n''); //printf(''This is containing the printf debug command\r\n''); while(1) { data = GetChar(); SerialPutChar(data); }} #stm32f103-usart2014-01-06 7:39 AM
I'd definitely front test for TXE before blind writing the data register.
Don't park a register view over the USART peripheral in the debugger. At first glance the code doesn't look bad.2014-01-06 11:47 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.