2016-05-09 12:13 AM
Hi,
i have problem with the CAN bus on a STM32F103C8 (48 pin). I configed the CAN and after the first transmit the bus went to Error and BusOFF state. The I checked the CAN Error status register and the TEC counter is full and the Last Error Code is: Bit dominant Error. I tried in loopback mode the software and then it runs well without error. I tried it with an STM32F103CB and with an STM32F103RB(64 pin), which is on a different hardware and it works in the same way and the bus will be off. So i thint it is a software problem and not both hardware is wrong. Here is my source code: int main(void) { NVIC_InitTypeDef NVIC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; CAN_InitTypeDef CAN_InitStructure; CAN_FilterInitTypeDef CAN_FilterInitStructure; RCC_ClocksTypeDef rcc; CanTxMsg TxMessage; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); RCC_GetClocksFreq(&rcc); /* GPIO clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); /* Configure CAN pin: RX */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configure CAN pin: TX */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinRemapConfig(GPIO_Remap1_CAN1 , ENABLE); NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* CAN register init */ CAN_DeInit(CAN1); CAN_StructInit(&CAN_InitStructure); /* CAN cell init */ CAN_InitStructure.CAN_TTCM = DISABLE; CAN_InitStructure.CAN_ABOM = DISABLE; CAN_InitStructure.CAN_AWUM = DISABLE; CAN_InitStructure.CAN_NART = DISABLE; CAN_InitStructure.CAN_RFLM = DISABLE; CAN_InitStructure.CAN_TXFP = DISABLE; //CAN_InitStructure.CAN_Mode = CAN_Mode_LoopBack; CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; /* CAN Baudrate = 0.5MBps*/ CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; CAN_InitStructure.CAN_BS1 = CAN_BS1_15tq; CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq; CAN_InitStructure.CAN_Prescaler = 4; CAN_Init(CAN1, &CAN_InitStructure); /* CAN filter init */ CAN_FilterInitStructure.CAN_FilterNumber = 0; CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask; CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit; CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0; CAN_FilterInitStructure.CAN_FilterActivation = ENABLE; CAN_FilterInit(&CAN_FilterInitStructure); CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); /* Transmit */ TxMessage.StdId = 0x321; TxMessage.ExtId = 0x01; TxMessage.RTR = CAN_RTR_DATA; TxMessage.IDE = CAN_ID_STD; TxMessage.DLC = 1; TxMessage.Data[0] = 1; uint32_t i = 0; /* Infinite loop */ while (1) { CAN_Transmit(CAN1, &TxMessage); for(i=0;i<50000;i++){} } } #stm32f103-can-bit-dominant-error2016-05-10 3:58 AM
/* CAN Baudrate = 1MBps*/
CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1 = CAN_BS1_3tq;//iriginally 3tq
CAN_InitStructure.CAN_BS2 = CAN_BS2_5tq;//originally 5tq
CAN_InitStructure.CAN_Prescaler = 4;//was 4 for 72Mhz clk
CAN_Init(CANx, &CAN_InitStructure);
2016-05-10 5:26 AM
The APB1 in this case would be 36 MHz
2016-05-10 8:50 AM
I assume you have also got the obvious 120 Ohm resistor at either end...? That will definitely cause issues in the real world if you haven't got them. The Sample point should also be around 75-90%.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.