2012-07-27 7:51 AM
Hello
I have read the core documents on the NVIC and it says that you can have a mix of pre emption priority and sub priority, for example you could have 2 pre emption and 6 sub priority levels. The data sheet for the STM32F105 stated that you can have 16 priority levels (4 bits of interrupt of priority are used - this can also be a mix of pre emption and sub priority levels). Which one is correct and if I use the method in the STMF105 data sheet, would I write the interrupt levels to trhe most or least significant nibble of the register i.e. NVIC->IPR[PREG_USART2] |= (unsigned long) (0x03 << PBIT_USART2); or NVIC->IPR[PREG_USART2] |= (unsigned long) (0x30 << PBIT_USART2); to set up Uart to as interrupt level 3 Cheers Peter2012-07-27 9:44 AM
The latter.
''Each priority field holds a priority value, 0-255. The lower the value, the greater the priority of the corresponding interrupt. The processor implements only bits[7:4] of each field, bits[3:0] read as zero and ignore writes.''
2012-07-30 1:46 AM
Hi clive1
Thanks for clearing that up, I am new to the device consequently still trying to find my way through the technicalities. Cheers PeterWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.