STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC or DMA issue with stm32f0_stdperiph_lib example

Posted on July 30, 2012 at 20:11I am trying to run the RTC and ADC_DMA example code together on my http://www.st.com/internet/evalboard/product/252994.jsp board.  I adjusted the code to remove the LCD display and send the ADC data output to the cons...

mvonahnen by Associate III
  • 778 Views
  • 1 replies
  • 0 kudos

Problem with relocating code to 0x0800 0400

Posted on July 29, 2012 at 22:28Hello everyone, thanks for reading the post. For STM32 : I am running into an issue when I try to run my code from 0x08000400 instead of 0x08000000. I am using IAR tools. As soon as I execute the statement the system...

ajit by Associate
  • 1241 Views
  • 2 replies
  • 0 kudos

CAN Bus Example

Posted on July 30, 2012 at 11:03hello, Can you please give a CAN bus Example for STM32F407. I don't know how to initialize and configure CAN protocol in STM32.Thanks.

STM32F102 and NVIC

Posted on July 27, 2012 at 16:51Hello I have read the core documents on the NVIC and it says that you can have a mix of pre emption priority and sub priority, for example you could have 2 pre emption and 6 sub priority levels. The data sheet for th...

pcoleman by Associate
  • 1392 Views
  • 2 replies
  • 0 kudos

Connect with LM75 through I2C/DMA on ST32100B

Posted on July 16, 2012 at 11:28 Hi, I am try to develop a simple I2C “receive data�? type of function; I took most of the code from the zip file that I was able to download from the st webpages. The main function of interest getBytesI2C1DMA(...

ptumati by Associate II
  • 1727 Views
  • 1 replies
  • 0 kudos

stm32f103VE enc28j60

Posted on July 27, 2012 at 18:30Hi, I try to connect a enc28j60( ethernet controler) with my stm32f103ve , but all exemples find in web don't work fine. some one to tell an exemple for this? thanks  

Implement USB host for full-speed HID gamepad

Posted on July 25, 2012 at 10:12i was implement USB host for Low-Speed HID gamepad (Discovery board) .... very good. But with gamepad Logitech Full-Speed...it not worki was debug grxsts.b.pktsts ( in interrupt callback USB_OTG_USBH_handle_rx_qlvl_IS...

STM32 Powered through SPI

Posted on July 27, 2012 at 16:10Hello,I have two STM32 chips, one as Master and one as Slave on separate power domains of 3.3V each. My problem is that when the Slave is turned off and power is removed, it is still being powered from the SPI Master....

Popcorn by Associate II
  • 2837 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.