2018-12-16 5:57 PM
recently I used the STM32F072 USRT3 to communicate with my peripheral, the configuration of USART3 is follow:
static void USART3_Init( void )
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable GPIO clocks */
RCC_APB1PeriphClockCmd(RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOB, ENABLE);
/* Enable USART3 clock */
USER_USART3_APBPERIPHCLOCK(USER_USART3_CLK, ENABLE);
/**USART3 GPIO Configuration
PB10 ------> USART3_TX
PB11 ------> USART3_RX
*/
/* Configure USART Tx and Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10|GPIO_Pin_11;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Enable SC_USART IRQ */
NVIC_InitStructure.NVIC_IRQChannel = USER_USART3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
USART_DeInit(USER_USART3);
/*Configure the initial baudrate*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_Init(USER_USART3, &USART_InitStructure);
USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
USART_ITConfig(USART3, USART_IT_IDLE, ENABLE);
USART_ReceiveData(USART3); //clear the RXNE pending bit
USART_ClearITPendingBit(USART3, USART_IT_IDLE);
/* Enable SC_USART */
USART_Cmd(USER_USART3, ENABLE);
}
the interrupt function is :
void USART3_4_IRQHandler( void )
{
if(USART_GetITStatus(USER_USART3, USART_IT_RXNE) != RESET)
{
/* Disable USER_USART3 RXNE Interrupt */
USART_ITConfig(USER_USART3, USART_IT_RXNE, DISABLE);
USART_ReceiveData(USER_USART3);
}
}
as I start to debug ,the value of: USART_GetITStatus(USART3, USART_FLAG_RXNE) is SET�? but ,I don't send any data to the STM32F072 device, why the interrupt flag is SET?
Solved! Go to Solution.
2018-12-18 10:27 PM
What I mean is that now you first enable interrupts and then clear the possible causes. And if there happens to be bits set in the received data register (that's possible after enabling the USART), the interrupt takes place right after enabling the interrupts and before the read.
Due to the pipeline, it might be a good idea to put DSB (barrier) between clearing the interrupt causes and enabling interrupts. I once had a problem, when in the beginning I first cleared interrupt conditions, then interrupts and then enabled the interrupts. The clearing of the interrupts didn't take effect early enough, so the execution ended up in the interrupt service with interrupt flag cleared. Putting a DSB in between the flag clearing and interrupt enabling fixed it.
2018-12-16 7:58 PM
Not sure I can unmuddle this.
#defines not provided and used inconsistently
AHB device clocks not enabled via APB1
AF pin sources not muxed properly
2018-12-16 8:58 PM
Not sure. but:
USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
USART_ITConfig(USART3, USART_IT_IDLE, ENABLE);
USART_ReceiveData(USART3); //clear the RXNE pending bit
USART_ClearITPendingBit(USART3, USART_IT_IDLE);
Try reordering these - clear interrupts before enabling. Maybe even DSB between.
2018-12-16 9:39 PM
the global definition of this as show below:
#define USER_USART3 USART3
#define USER_USART3_CLK RCC_APB1Periph_USART3
#define USER_USART3_APBPERIPHCLOCK RCC_APB1PeriphClockCmd
#define USER_USART3_IRQn USART3_4_IRQn
#define USER_USART3_4_IRQHandler USART3_4_IRQHandler
2018-12-16 9:43 PM
the global definition of this as show below:
#define USER_USART3 USART3
#define USER_USART3_CLK RCC_APB1Periph_USART3
#define USER_USART3_APBPERIPHCLOCK RCC_APB1PeriphClockCmd
#define USER_USART3_IRQn USART3_4_IRQn
#define USER_USART3_4_IRQHandler USART3_4_IRQHandler
if this not work, can you offer a template sample code about STM32F072 USART3 ?
2018-12-18 10:27 PM
What I mean is that now you first enable interrupts and then clear the possible causes. And if there happens to be bits set in the received data register (that's possible after enabling the USART), the interrupt takes place right after enabling the interrupts and before the read.
Due to the pipeline, it might be a good idea to put DSB (barrier) between clearing the interrupt causes and enabling interrupts. I once had a problem, when in the beginning I first cleared interrupt conditions, then interrupts and then enabled the interrupts. The clearing of the interrupts didn't take effect early enough, so the execution ended up in the interrupt service with interrupt flag cleared. Putting a DSB in between the flag clearing and interrupt enabling fixed it.
2018-12-19 2:55 AM
Thank you very much,the problem had been solved yet
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.