2015-11-23 2:49 PM
Dear ST community,
I�m using STM32F072CB, standard peripheral library and �STMTouch_Lib_V1.1.0� the problem is in the Touch library, I copied the example �STM32F0518_Ex01_3TKeys_EVAL� in my working project since it is exactly what I want to add to my current project(3 touch keys), I modified the configuration file to fit my application but nothing working so it is either I did something wrong in my modifications or I missed something else, anyone can help?
My PCB is designed to use only Group 1 with the following configuration
G1_IO1 --> Ref. Capacitor of 33nF
G1_IO2 --> Touch Key
G1_IO3 --> Touch Key
G1_IO4 --> Touch Key
No Shield.
I�m also attaching the configuration file.
Best regards,
Mina Anton
#touch #stm32f0 #capacitivetouch2015-11-24 2:46 AM
Hi anton.mina,
It seems you didn't attached the configuration file. Could you please add it?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.