2026-03-17 12:22 AM - edited 2026-03-17 12:45 AM
Hi,
Having just updated to STM32CubeIDE 2.1.1, I've created an STM32CubeIDE Empty Project (the only apparent relevant option) targeting the STM32F072 Discovery Kit as I want to experiment with the touch sensing capabilities, however when the project is created I don't see an IOC file.
Has the workflow reverted to using STM32CubeMX to create the IOC file etc. please?
Kind regards,
Al
Solved! Go to Solution.
2026-03-17 12:56 AM
Hello @alw
from the STM32CubIDE V2.0.0, the STM32CubeMX plug-in has been removed. So, the .ioc file is opened out of the STM32CubeIDE on the standalone version of the STM32CubeMX.
see STM32CubeIDE 2.0.0 released.
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-17 12:53 AM
So apparently functionality removed form STM32CubeIDE which seems like a backwards step...
2026-03-17 12:56 AM
Hello @alw
from the STM32CubIDE V2.0.0, the STM32CubeMX plug-in has been removed. So, the .ioc file is opened out of the STM32CubeIDE on the standalone version of the STM32CubeMX.
see STM32CubeIDE 2.0.0 released.
BR
Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-03-17 4:27 AM - edited 2026-03-19 3:27 AM
@alw wrote:So apparently functionality removed form STM32CubeIDE which seems like a backwards step...
It was also announced ahead of the v2.0.0 release: STM32CubeIDE 2.0 release - early heads-up!
See Version 2.0.0 - why remove MX ? for discussion and more on the rationale.
Note also: Introducing STM32CubeMX2, a new flavour of STM32CubeMX tool - having both integrated is probably impractical, so having both separate makes more sense ...
2026-03-18 7:16 PM
2026-03-19 3:31 AM
Ha ha! Brilliant - I'm stealing that!
2026-05-14 6:11 AM
... it is not the solution how to create the *.ioc-File also for version 2.x but only the explanation why it is not there anymore! :(
2026-05-14 6:45 AM
If you read the linked article, it explains that CubeMX is used to create the .ioc file, and the OP already hinted at that.
See also: STM32CubeIDE 2.0.0 New workflow tutorial.
2026-05-15 1:57 AM
...maybe the link is interesting for people who use CubeMX, I don't.
The original reason why I searched for the *.ioc-file was a hint somewhere in the internet that in order to create a terminal window for debug reasons you can write something into the *.ioc-file.
But I found another solution: I installed plugins for the topic terminal and then could create one at "window/show view/others->terminal. After configuring for my FTDI-USB modul (Baud rate etc) it worked fine.
But thanks for your comment!
2026-05-15 2:10 AM - edited 2026-05-15 2:11 AM
Well, if you want an .ioc file, then you do have to use CubeMX* - the .ioc file is the CubeMX file.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.