STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 CMSIS Std Periph Library Available?

Posted on November 23, 2015 at 22:28Hi, Can someone please advise on the availability of the std peripheral libraries for the STM32L4 device? That is, HAL-free?  I couldn't find any in the package that i got from the ST website that claims there is ...

RS485 modbus Communication with Nucleo

Posted on November 24, 2015 at 17:05Hello Everyone.I would use the NUCLEO l152re board to implement the Modbus via RS485 and communicate with one or more slaves.Right now I would need of MODBUS master library for STM32 NUCLEO.Is there anyone that ca...

DMX-512 RECEIVER

Posted on November 24, 2015 at 17:03HiI'm trying to receive dmx512 with a stm32f100rb (discovery board). I can't detect the break. Please help me :'(I try to detect the break with timers but my results are bad.... If someone can explain me how to de...

Problem loading code

Posted on November 24, 2015 at 09:51Hello,I' m programming stm32f103RB and my code goes well but I'm doing some changes and when I try to load the code the IAR show my this error:* Programming failed @address 0x0800400 (program error)I don't know wh...

msanchez by Associate II
  • 1000 Views
  • 1 replies
  • 0 kudos

''addend register'' value calculation (for PTP)

Posted on November 16, 2015 at 07:49http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/PF257871?s_searchtype=keywordI am confused about ''addend register'' value calculation. From reference manual: addend = 2^32 / FreqDivisionRatio; Fr...

Andrew1 by Associate II
  • 991 Views
  • 1 replies
  • 0 kudos

Concurrent GPIO access from threads and ISR

Posted on November 20, 2015 at 02:25In my Stm32F4 applicarion, I am using (a.o.) sw4stm32, cubemx and Freertos. Some of the GPIO I need to access from different threads and even from from ISR. Access means, changing port state, reading port state, r...

STM32F072 Capacitive Touch

Posted on November 23, 2015 at 23:49Dear ST community,I�m using STM32F072CB, standard peripheral library and �STMTouch_Lib_V1.1.0� the problem is in the Touch library, I copied the example �STM32F0518_Ex01_3TKeys_EVAL� in my working project since it...

MMU unit enable in STM32F7

Posted on November 20, 2015 at 22:05Hello. I have noticed that in the cubef7 examples many projects starts with MPU_Config() function . Is it necessary to use MPU unit in STM32F7? And the same question about L1 cache. Can i don't use it? Thank you.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.