2019-01-09 1:46 AM
I have a problem on a STM32F071C board. The PLL will not reach ready state. I am using the HSI and in order to reduce current consumption I want to devide PLL from 8MHz down to 2MHz. This works fine on most board (18 out of 20) but on some the PLL_RDY is never set. Do I violate any requirements by using RCC->CFGR2 = RCC_CFGR2_PREDIV_DIV4?
/* Enable Prefetch Buffer and set Flash Latency */
FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;
/* HCLK = SYSCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_HPRE_DIV1;
/* PCLK = HCLK */
RCC->CFGR |= (uint32_t)RCC_CFGR_PPRE_DIV1;
/* PLL configuration = HSI * 2 = 4 MHz */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_PLLSRC | RCC_CFGR_PLLXTPRE | RCC_CFGR_PLLMUL));
RCC->CFGR |= (uint32_t)(RCC_CFGR_PLLSRC_HSI_PREDIV | RCC_CFGR_PLLMUL2);
RCC->CFGR2 = RCC_CFGR2_PREDIV_DIV4;
/* Enable PLL */
RCC->CR |= RCC_CR_PLLON;
/* Wait till PLL is ready */
while((RCC->CR & RCC_CR_PLLRDY) == 0)
{
}
/* Select PLL as system clock source */
RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));
RCC->CFGR |= (uint32_t)RCC_CFGR_SW_PLL;
/* Wait till PLL is used as system clock source */
while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)
{
}
Solved! Go to Solution.
2019-01-09 3:31 AM
As a comment, I don't like the way you modify RCC->CFGR, doing it in two hits with the first to clear some bits and the second to set others.
Looking at the data sheet section 6.3.9, I think the PLL should be able to sing between 16 and 48 MHz. So maybe getting the PLL to run at 8 MHz is outside the specification, and you have to run it at 16 MHz and divide by 2 (or whatever you want) to get HCLK.
Hope this helps,
Danish
2019-01-09 3:31 AM
As a comment, I don't like the way you modify RCC->CFGR, doing it in two hits with the first to clear some bits and the second to set others.
Looking at the data sheet section 6.3.9, I think the PLL should be able to sing between 16 and 48 MHz. So maybe getting the PLL to run at 8 MHz is outside the specification, and you have to run it at 16 MHz and divide by 2 (or whatever you want) to get HCLK.
Hope this helps,
Danish
2019-01-09 4:11 AM
You are right, I only checked the PLL input frequency which is ok down to 1 MHz but the min output frequency is 16 MHz. That is probably the problem.
Thanks!
2019-01-09 5:38 AM
Why do you need PLL at all? Use HSI16 with AHB Prescaler 2 to get 8 MHz.
2019-01-09 6:47 AM
I am now running directly out of the HSI8 and PLL turned off. Problem solved!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.