2016-10-03 12:22 PM
Hi all,
I'm developing a solution with a STM32F030 and a serial-to-WiFi module SPWF01SA. I downloaded the expansion package X-CUBE-WIFI1 from ST website that provides sample implementations for others NUCLEO like as STM32L0, L4, F1 and F4. I started from STM32L0 sample and changed the some function/registers to the STM32F0, but I'm having some problems... First, a lot of UART data were being lost in the reception, then when I commented the lines that disabled the interruption before pop a byte from the circular buffer in the queue: //__disable_irq(); WiFi_Counter_Variables.temp = pop_buffer_queue(&wifi_instances.big_buff); //contents of temp(pop_buffer) will not change till another de-queue is made //__enable_irq(); This improved a lot, it seemed that I had solved, but some bytes are being lost yet. I think it is something in the software, beetween the push queue and pop queue from serial UART. I tried to change the interruption priority from UART(push data) and Systick (pop data). Also change the interruption frequency, but nothing worked. I don't have much experience with queues. Do you have some tips to help me? It will be very usefull if ST provide an update for X-CUBE-WIFI1 with SMT32F0. Because the STEVAL-IDW001V1 software library isoutdated.
Thanks in advance. #x-cube-wifi1-smt32f0-spwf01sa2016-10-04 5:29 AM
Hi Guilherme Thome,
Thank you for these feedbacks. But what do you mean by outdated ?-Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.