2016-10-03 10:17 PM
Hello, everyone.
AccessPort app was used for test. AccessPort prints ''0x00, 0x55, 0x55, 0x55, 0x55, 0x55, 0x79, 0x3D'' Test code is as follows; int main(void) { char szTemp[8] = {0x55, 0x55, 0x55, 0x55, 0x55, 0x0D, 0x0A, 0}; uart_init(); led_init(); //Uart_SendString(''hello STM32F205..!!!\r\n\0''); Uart_SendString(szTemp); /* Infinite loop */ while (1) { Delay_ms(500); GPIOC->BSRRH |= (1 << 2); Delay_ms(500); GPIOC->BSRRL |= (1 << 2); } }2016-10-04 4:47 AM
What is ''AccessPort app''? And what exactly is the problem?
JW2016-10-04 6:14 AM
Assume for a second it is not an issue with the code shown, show the code that actually outputs the string.
Use a debugger, confirm that the static data in memory reflects the data you expect to be sent.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.