2015-09-01 3:03 AM
Hello,
I am trying to send data to a computer with an HC 06 linked to an STM32F0 Discovery.Here is my code :/* USART2 PA.2 Tx, PA.3 Rx STM32F0-Discovery*/
/* Includes ------------------------------------------------------------------*/ #include ''main.h'' #include ''stdio.h'' /* Private variables ---------------------------------------------------------*/ /* Functions prototypes ---------------------------------------------------------*/ void RCC_Configuration(void) { RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /*Activation des clocks de l'usart2 et du port A*/ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); } void configUSART2 (void) { USART_InitTypeDef USART_InitStructure; USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2,ENABLE); } void configGPIOA (void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1); } void Usart2Send(uint8_t data) { USART_SendData(USART2, (uint8_t) data); //Loop until the end of transmission while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET)// Wait for Empty { } } void outstring(char *s) { while(*s) { /* Loop until transmit data register is empty */ while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET)// Wait for Empty USART_SendData(USART2, (uint8_t)*s++); } } uint8_t Usart2Read(void){ while ( USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET); return (uint8_t)USART_ReceiveData(USART2); } int main(void) { RCC_Configuration(); configUSART2(); configGPIOA(); Usart2Send('A'); Usart2Send('T'); while(1) { } } Here is what i get on Putty :▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒AT▒▒▒▒▒
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒n▒▒▒
▒▒▒▒▒▒▒▒▒▒▒▒Ǡ▒̸▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒l▒▒▒
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒A
I configured on keil on putty the same parameters : 9600baud, 8 bits data, 1 bit stop, no parity and no verification.Any idea ? (by the way, I did not find how to put my code properly on the forum, sorry about that).Thanks in advance2015-09-01 9:17 AM
The Format Code Block tools is the Paintbrush [<>] icon, top left of the Word-in-a-box(tm) interface.
The HC-06 might need configuring at the STM32 end, sending ''AT'' command (no CR/LF) and waiting is the way of getting into command mode, as I recall, not sure you'd get that data over the air once it switches out of data mode.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.