STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART Bootloader Protocol- Read command

Posted on September 01, 2015 at 14:24I have an STM32F4 Discovery board and I'm trying to talk to the boot loader.  I have brought it up and I have successfully executed the 'Get', and 'Get Version and Read Protection Status' commands.  When I try th...

ttatakis by Associate III
  • 2071 Views
  • 4 replies
  • 0 kudos

STM32F05x IAP flash page erase, pending ISR

Posted on September 01, 2015 at 18:36Hello, i use EEPROM simulation and sometime i must use the flash page erase for new data. If during the erase time there is one ore more pending ISR, the system crashed. After reboot with the watchdog i found, th...

ingo by Associate II
  • 1214 Views
  • 2 replies
  • 0 kudos

STM32F0 and HC 06

Posted on September 01, 2015 at 12:03Hello,I am trying to send data to a computer with an HC 06 linked to an STM32F0 Discovery.Here is my code :  /* USART2 PA.2 Tx, PA.3 Rx STM32F0-Discovery*/ /* Includes ----------------------------------------...

edouard by Associate II
  • 1126 Views
  • 1 replies
  • 0 kudos

STM32 F4 to F7 code migration

Posted on September 01, 2015 at 11:16Hello. I am trying to run the code from stm32f429 to stm32f746. There is one question. DTCM memory (cortex m7) and CCM memory (cortex m4) is the same? 

STM32CubeMX RTC code generation: probably a bug?

Posted on August 30, 2015 at 22:14 On the STM32L051 I was trying to use the WKUP1 pin to wake up the processor from standby mode. Too bad I didn't notice the fact that a pulldown is enabled on that pin.... So now I'm trying to play this t...

bart2 by Associate II
  • 1165 Views
  • 1 replies
  • 0 kudos

[SOLVED]storing struct into flash

Posted on August 31, 2015 at 11:04 Hello I am trying to save my settings into flash. I use a struct that storing settings, then put a pointer begining of it and store all the bytes into flash along the size of that struct. But it seems struc...

STM32F303 - Changing PWM mode on the fly

Posted on August 31, 2015 at 17:45 Hi, I use TIM1 PWM in asymmetric mode. I need to switch between 2 software modes : Mode A - CH1/1N asym mode 2, CH3/3N asym mode 2 Mode B - CH1 asym mode 1, CH3 asym mode 2, CH1N/3N off ...

danny2 by Associate
  • 1512 Views
  • 2 replies
  • 0 kudos

STM32F205 , 64 pin, breakout board

Posted on August 26, 2015 at 10:341. Is there any breakout board available for STm32F205RBT6?2. I had some issues with my MCU, which I couldn't resolve: http://tinyurl.com/qf7jguw(thread: SWD floats, STM32F2, code don't run)3. Problem could be in bo...

STM32F072 - Proper USB interface circuit

Posted on September 01, 2015 at 04:11Hello! I am developing using the STM32F072C8T6.  I was hoping to use USB communication and the hardwired boot loader for initial programming of the chips.  I am running into some issues, however, and was wonderin...

crwest by Associate
  • 853 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.