2013-01-27 6:58 AM
Hi,
I am trying to play some audio on my evaluation board,but no luck : I have a buffer that contain slices from various wav files,the buffer located in the external RAM ( if it matters) , and i try to do the following :EVAL_AUDIO_Init(OUTPUT_DEVICE_AUTO, DEFAULT_VOLMAX, I2S_AudioFreq_44k);
EVAL_AUDIO_Play((uint16_t*)data,audioChunkSize/2); // data is my buffer
Any ideas what maybe i am doing wrong?
Thanks
2013-01-27 7:01 AM
Also , after the
EVAL_AUDIO_Play((uint16_t*)data,audioChunkSize/2); // data is my buffer execution ,i do enter the callback function : EVAL_AUDIO_TransferComplete_CallBack
but no sound whatsoever.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.